请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5149 工具与软件:
因为 LM5149能够 使用高于5V 的米勒钳位电压驱动 MOSFET? 此外、对于建议栅极驱动电压为12V 的 MOSFET、我们是否能够为此采用外部栅极驱动器电路?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.