工具与软件:
您好!
我使用 LM5010制作12V 降压设计。 这非常复杂、因为它以-48V 为基准。 转换器以大约0.5A 的总成本为两个风扇供电。 有时转换器根本就无法正常工作。
故障的根本原因可能是什么?
输入电压范围:-40V 至-60V
原理图:
扼流圈详细信息:CLF10040T-101M-D
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.