请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5155-Q1 主题中讨论的其他器件:LM5155
工具与软件:
LM5155做反激升压的架构应用、12V 升压到60V
调试中、在MOS管开启瞬间、变压器副边输出会有 º C 至100V以上的负压。如何降低这个负压 º C
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.