请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ51051B 主题中讨论的其他器件:TIDA-00318
工具与软件:
你(们)好
我们是否有集成无线/线功能的合适蓄电池充电器?
线充状态:μ s
- 电池容量2000 mA 4.12.4.
- 电池充电电压:4.35V
- 充电电流:0.5C (1A)
无线条件:
- 符合 Qi 标准15W 1A 充电2000 mA。Ω 电池
BRS
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
你(们)好
我们是否有集成无线/线功能的合适蓄电池充电器?
线充状态:μ s
无线条件:
BRS
Brian