请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCD9248 工具与软件:
我需要 SEQ 引脚如何工作在这个 IC 中,如果有三个 PMIC 的 ucd9248和如果 SEQ 引脚短路如何可以用于配置,以及什么8相在数据表提到,如果只有四个通道可以使用为什么他们8通道
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.