Other Parts Discussed in Thread: UCC28221
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28221 工具与软件:
您好!
我打算在交错升压转换器应用中使用 UCC28221。 为了限制启动期间的浪涌电流、我想将占空比钳制为某个最小值(假设为10%)。 是否可以通过调整引脚10 (CHG)和引脚9 (DISCHG)上的电阻器来实现该低占空比? 谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.