请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLV761 工具与软件:
电源12V、负载电流设置为300mA、持续10秒、输出电压将下拉至0V、过热保护。
我的问题是、为什么电源容量小于500mA、甚至是1A?
规格上的1A 指的是什么? 
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
电源12V、负载电流设置为300mA、持续10秒、输出电压将下拉至0V、过热保护。
我的问题是、为什么电源容量小于500mA、甚至是1A?
规格上的1A 指的是什么?