Other Parts Discussed in Thread: TPS82130
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS82130 工具与软件:
嗨、团队:
我想问一下 TPS82130的输出电压。 在下面的屏幕截图中、输出范围是0.9V-6V、但 FB 电压为0.8V。 输出比 FB 高100mV。
这种使用的原因是什么? 如果它低于0.9V、是否存在任何风险? 谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.