Other Parts Discussed in Thread: LP5018
工具与软件:
使用条件:
在 VCC = 5V 时使用
工作环境为85°C
数据表中 ILIM 的说明指出其提到120mA。
如果驱动 LED 的总电流为120mA、这是否可以接受?
如果超过120mA、可能会出现什么样的问题?
如果总电流超过120mA、是否可以在提供热辐射解决方案的情况下使用 LED?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.