This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SK-AM64B:USB DFU 引导

Guru**** 2558250 points
Other Parts Discussed in Thread: SK-AM64B

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1274375/sk-am64b-usb-dfu-boot

器件型号:SK-AM64B

您好!

我在使用 ti-SDK 版本 AM64XX 09_00_00_03时尝试从 USB DFU 引导。

我要通过单击下方链接来完成此操作。

https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/09_00_00_03/exports/docs/linux/Foundational_Components Boot/UG-DFU.html

加载 tiboot3.bin 时出错、如下所示。

U-Boot SPL 2023.04-00001-g4446269d4e-dirty (Sep 25 2023 - 19:50:10 +0530)
EEPROM not available at 0x50, trying to read at 0x51
Resetting on cold boot to workaround ErrataID:i2331
Please resend tiboot3.bin in case of UART/DFU boot
resetting ...

U-Boot SPL 2023.04-00001-g4446269d4e-dirty (Sep 25 2023 - 19:50:10 +0530)
EEPROM not available at 0x50, trying to read at 0x51
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13376 bytes
Trying to boot from DFU
No USB device found
usb_gadget_initialize failed
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
 

如果需要任何详细信息、请告诉我!

此致、

达米克

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Dharmik:

    SK-AM64B USB 端口配置为仅主机模式、它不支持 DFU 引导模式。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的答复。

    我们对 SK-AM64B 板的 USB 部分进行了修改、使其像  AM64x GPEVM 一样、因为它支持 DFU。  

    返工如下所述、

    1) 1)已删除 R267

    2) 2)删除了 U48

    我们已从 EVM 中移除 R267和 U48以将 SoC USB 端口配置为器件。

    如果 在硬件和软件方面还有任何缺失、敬请告知。

    此致、

    达米克

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    通过以下修改、我们可以使用 dfu-util 实用程序加载 tiboot3.bin 和 tispl.bin

    diff --git a/arch/arm/dts/k3-am64-main.dtsi b/arch/arm/dts/k3-am64-main.dtsi
    index 5e8036f32d..e767709de9 100644
    --- a/arch/arm/dts/k3-am64-main.dtsi
    +++ b/arch/arm/dts/k3-am64-main.dtsi
    @@ -616,7 +616,7 @@
                                              "peripheral",
                                              "otg";
                            maximum-speed = "super-speed";
    -                       dr_mode = "otg";
    +                       dr_mode = "peripheral";
                    };
            };
    
    diff --git a/arch/arm/dts/k3-am642-sk-u-boot.dtsi b/arch/arm/dts/k3-am642-sk-u-boot.dtsi
    index f9393e098a..484592772c 100644
    --- a/arch/arm/dts/k3-am642-sk-u-boot.dtsi
    +++ b/arch/arm/dts/k3-am642-sk-u-boot.dtsi
    @@ -245,7 +245,7 @@
     };
    
     &usb0 {
    -       dr_mode = "host";
    +       dr_mode = "peripheral";
            bootph-pre-ram;
     };
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    使用上述补丁加载 tispl.bin 后、似乎与主机的 DFU 连接丢失、无法加载 u-boot。


    我们已将来自 sudo dfu-util -a u-boot.img -D u-boot.img 我们用来尝试加载 u-boot.img 的命令。

    1)主机,

    dfu-util 0.11
    
    Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
    Copyright 2010-2021 Tormod Volden and Stefan Schmidt
    This program is Free Software and has ABSOLUTELY NO WARRANTY
    Please report bugs to sourceforge.net/.../
    
    dfu-util: Warning: Invalid DFU suffix signature
    dfu-util: A valid DFU suffix will be required in a future dfu-util release
    dfu-util: No DFU capable USB device available

    2) SK-AM64B 板、

    U-Boot SPL 2023.04-00001-g4446269d4e-dirty (Sep 26 2023 - 16:48:23 +0530)
    EEPROM not available at 0x50, trying to read at 0x51
    Resetting on cold boot to workaround ErrataID:i2331
    Please resend tiboot3.bin in case of UART/DFU boot
    resetting ...
    
    U-Boot SPL 2023.04-00001-g4446269d4e-dirty (Sep 26 2023 - 16:48:23 +0530)
    EEPROM not available at 0x50, trying to read at 0x51
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    SPL initial stack usage: 13376 bytes
    Trying to boot from DFU
    ##########################################DOWNLOAD ... OK
    Ctrl+C to exit ...
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Loading Environment from MMC... MMC Device 0 not found
    *** Warning - No MMC card found, using default environment
    
    init_env from device 10 not supported!
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb
    NOTICE:  BL31: Built : 11:57:41, Sep 13 2023
    I/TC:
    I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.1 20220712 (Arm GNU Toolchain 11.3.Rel1)) #1 Mon Sep 25 13:35:06 UTC 2023 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    I/TC: HUK Initialized
    I/TC: Activated SA2UL device
    I/TC: Enabled firewalls for SA2UL TRNG device
    I/TC: SA2UL TRNG initialized
    I/TC: SA2UL Drivers initialized
    I/TC: Primary CPU switching to normal world boot
    
    U-Boot SPL 2023.04-00001-g4446269d4e-dirty (Sep 26 2023 - 17:49:53 +0530)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    Trying to boot from DFU

    返工似乎正常工作;我们是否缺少任何与 SDK 相关的信息?  

    此致、

    达米克

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Dharmik:

    您能否使用 Processor SDK v8.4进行测试?

    我测试 DFU 的上一个 SDK 版本是 v8.4、尚未使用 SDK9.0测试 DFU。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我还使用 SDK 版本8.6进行测试、但结果是相同的、我尝试使用 SDK 版本8.4进行构建和测试。

    为了从 DFU USB 引导、我需要进行哪些更改。  

    您愿意与我分享这些补丁或步骤吗?

    此致、

    达米克

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Dharmik:

    在 SDK8.6中、DFU 已知断开。 请参阅以下常见问题解答:

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1206531/faq-am625-linux-sdk-v08-06-u-boot-usb-dfu-boot-is-broken-with-dfu_alt_info_ram-env-variable-not-defined-error

    尽管该常见问题解答提到了 AM62x、但问题和解决方案也适用于 AM64x。