您好!
我在使用 ti-SDK 版本 AM64XX 09_00_00_03时尝试从 USB DFU 引导。
我要通过单击下方链接来完成此操作。
加载 tiboot3.bin 时出错、如下所示。
U-Boot SPL 2023.04-00001-g4446269d4e-dirty (Sep 25 2023 - 19:50:10 +0530) EEPROM not available at 0x50, trying to read at 0x51 Resetting on cold boot to workaround ErrataID:i2331 Please resend tiboot3.bin in case of UART/DFU boot resetting ... U-Boot SPL 2023.04-00001-g4446269d4e-dirty (Sep 25 2023 - 19:50:10 +0530) EEPROM not available at 0x50, trying to read at 0x51 SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') SPL initial stack usage: 13376 bytes Trying to boot from DFU No USB device found usb_gadget_initialize failed SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
如果需要任何详细信息、请告诉我!
此致、
达米克