请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM5118、 LM5121工具/软件:WEBENCH设计工具
您好,
lm5118的输入和输出极性是否相反? 例如、我可以输入-48V、输出+9V 吗? 作为降压/升压电路、它应支持输入和输出的反极性。 为什么我的电路输出只有在输入电压为正时才正常+ 9V? 请帮助回答、谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.