This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352P:CC1352P1 &UART2写入帧错误

Guru**** 2611305 points
Other Parts Discussed in Thread: SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1337961/cc1352p-cc1352p1-uart2-write-frame-error

器件型号:CC1352P
主题中讨论的其他器件:SysConfig

我只是尝试使用 CC1352P1 LP 测试 UART 写入、我已经连接了一个逻辑分析仪以确保我发送的是正确的、似乎收到了帧错误。 我仅尝试使用 uartecho 示例代码 SDK 7.10.02.23发送 ASCII 字符"A"。 下面是 SysConfig、代码和逻辑分析仪捕获的屏幕截图。 导致数据错误的原因是  

/*
 * Copyright (c) 2020, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ======== uart2echo.c ========
 */
#include <stdint.h>
#include <stddef.h>

/* Driver Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/UART2.h>

/* Driver configuration */
#include "ti_drivers_config.h"

/*
 *  ======== mainThread ========
 */
void *mainThread(void *arg0)
{
    char input;
    const char echoPrompt[] = "B\r\n";
    UART2_Handle uart;
    UART2_Params uartParams;
    size_t bytesRead;
    size_t bytesWritten = 0;
    uint32_t status     = UART2_STATUS_SUCCESS;

    /* Call driver init functions */
    GPIO_init();

    /* Configure the LED pin */
    GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);

    /* Create a UART where the default read and write mode is BLOCKING */
    UART2_Params_init(&uartParams);
    uartParams.baudRate = 115200;
    uartParams.parityType = UART2_Parity_NONE;
    uartParams.stopBits = UART2_StopBits_1;
    uartParams.dataLength = UART2_DataLen_8;


    uart = UART2_open(CONFIG_UART2_1, &uartParams);

    if (uart == NULL)
    {
        /* UART2_open() failed */
        while (1) {}
    }

    /* Turn on user LED to indicate successful initialization */
    GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);

    UART2_write(uart, echoPrompt, sizeof(echoPrompt), &bytesWritten);

    return 0;
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Corey:

    我测试了您的代码,它似乎工作正常,因为终端程序没有抱怨。

    此致、

    亚瑟

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Arthur、  

    很抱歉、我忘记了说我是使用引脚25 (TX)尝试输出 UART、这是您能够在自己身边进行测试和仿真的东西。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Corey:

    即使在 DIO25上、我也能得到正确的结果:

    作为参考、这里是我的 SysConfig 文件:

    此致、

    亚瑟

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    可以。 我使用不同的逻辑分析仪和接收器进行了测试、结果正确。 谢谢你