Part Number: TMS320F28377S
My DC module configuration is as follows. I modified EPwm2Regs.SWVDELVAL in the interrupt, but the delay cannot be updated in a timely manner. Moreover, I observed the EPwm2Regs.HWVDELVAL value in CCS in real time, which is different from EPwm2Regs.SWVDELVAL.
EPwm2Regs.DCAHTRIPSEL.bit.TRIPINPUT4 = 1;//DCAH = TRIP4
EPwm2Regs.TZDCSEL.bit.DCAEVT1 = 2;//DCAH = high
EPwm2Regs.DCACTL.bit.EVT1SRCSEL = 1;
EPwm2Regs.DCACTL.bit.EVT1FRCSYNCSEL = 1;
EPwm2Regs.DCACTL.bit.EVT1SYNCE = 1;
//时间滤波
EPwm2Regs.DCFCTL.bit.SRCSEL = 0;
EPwm2Regs.DCFCTL.bit.EDGEFILTSEL = 1; //enable edge filter
EPwm2Regs.DCFCTL.bit.EDGEMODE = 0; //Edge Mode Select
EPwm2Regs.DCFCTL.bit.EDGECOUNT = 0; // Edge Count
EPwm2Regs.VCAPCTL.bit.TRIGSEL = 1;//
EPwm2Regs.VCAPCTL.bit.VCAPE = 1;//
EPwm2Regs.VCAPCTL.bit.EDGEFILTDLYSEL = 1;// DELAY
EPwm2Regs.VCAPCTL.bit.VDELAYDIV = 0;
EPwm2Regs.SWVDELVAL= Tdelay;
EPwm2Regs.DCFCTL.bit.BLANKE = 1;
EPwm2Regs.DCFCTL.bit.PULSESEL = 1;
EPwm2Regs.DCFOFFSET = 1;
EPwm2Regs.DCFWINDOW = 1;
EPwm2Regs.DCCAPCTL.bit.CAPE = 0;