This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问在CCS6.0环境下,怎样才能使用SEED-510PLUS仿真器成功连接TMS320F28335型数字信号处理器呢?



将SEED-510PLUS仿真器驱动安装在.//ccsv5/ccs_base下,重启CCS,connection中出现了SEED XDS510PLUS Emulator,但是debug后还是出现问题:


Error connecting to the target:
(Error -120 @ 0x0)
This error number is used when a command is invalid.
It is likely a problem with `SC_CMD' in SMG_call()
selecting a function that has not been implemented.
(Emulation package 5.1.450.0)


请教如何才能正确连接,难道3.3以上的版本都不支持SEED-510PLUS了吗?我安装了CCS3.3,可以成功连接上,但是感觉3.3的界面太不适应了,多谢大家的回复。