将SEED-510PLUS仿真器驱动安装在.//ccsv5/ccs_base下,重启CCS,connection中出现了SEED XDS510PLUS Emulator,但是debug后还是出现问题:
Error connecting to the target:
(Error -120 @ 0x0)
This error number is used when a command is invalid.
It is likely a problem with `SC_CMD' in SMG_call()
selecting a function that has not been implemented.
(Emulation package 5.1.450.0)
请教如何才能正确连接,难道3.3以上的版本都不支持SEED-510PLUS了吗?我安装了CCS3.3,可以成功连接上,但是感觉3.3的界面太不适应了,多谢大家的回复。