Multiple triggers as sources for the start-of-conversion (SOC) sequence
– S/W - software immediate start
– ePWM 1-6
– GPIO XINT2
Why XINT1 can start ADC (SOC mode) ???
为啥XINT1也能触发启动ADC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Multiple triggers as sources for the start-of-conversion (SOC) sequence
– S/W - software immediate start
– ePWM 1-6
– GPIO XINT2
Why XINT1 can start ADC (SOC mode) ???
为啥XINT1也能触发启动ADC
#include "DSP28x_Project.h"
interrupt void adc_isr(void);
interrupt void xint1_isr(void);
Uint16 Result = 0;
main()
{
InitSysCtrl();
EALLOW;
SysCtrlRegs.HISPCP.all = 3;
EDIS;
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW;
PieVectTable.ADCINT = &adc_isr;
PieVectTable.XINT1 = &xint1_isr;
EDIS;
InitAdc();
AdcRegs.ADCMAXCONV.all = 0x0000;
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0;// ADCINA0
AdcRegs.ADCTRL2.bit.EXT_SOC_SEQ1 = 1;
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1;
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0;// LED
GpioCtrlRegs.GPADIR.bit.GPIO0 = 1;
EDIS;
GpioDataRegs.GPASET.bit.GPIO0 = 1;
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 0;// XINT1
GpioCtrlRegs.GPADIR.bit.GPIO15 = 0;
GpioCtrlRegs.GPAPUD.bit.GPIO15 = 1;
GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 2;
GpioCtrlRegs.GPACTRL.bit.QUALPRD1 = 0xFF;
EDIS;
EALLOW;
GpioIntRegs.GPIOXINT1SEL.bit.GPIOSEL = 15;
EDIS;
XIntruptRegs.XINT1CR.bit.POLARITY = 1;
XIntruptRegs.XINT1CR.bit.ENABLE = 1;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
PieCtrlRegs.PIEIER1.bit.INTx4 = 1;
IER |= M_INT1;
EINT;
for(;;);
}
interrupt void adc_isr(void)
{
Result = AdcRegs.ADCRESULT0 >>4;
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
interrupt void xint1_isr(void)
{
GpioDataRegs.GPATOGGLE.bit.GPIO0 = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}