This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 ADC-SOC触发启动方式

Multiple triggers as sources for the start-of-conversion (SOC) sequence
– S/W - software immediate start
– ePWM 1-6
– GPIO XINT2

Why XINT1 can start ADC (SOC mode)  ???

为啥XINT1也能触发启动ADC

  • 原则上只有XINT2可以触发ADC转换,请问如何判断是XINT1触发的?

  • 我通过仿真,看到进入ADC中断

  • #include "DSP28x_Project.h"

    interrupt void adc_isr(void);
    interrupt void xint1_isr(void);

    Uint16 Result = 0;

    main()
    {
    InitSysCtrl();

    EALLOW;
    SysCtrlRegs.HISPCP.all = 3;
    EDIS;

    DINT;

    InitPieCtrl();

    IER = 0x0000;
    IFR = 0x0000;

    InitPieVectTable();

    EALLOW;
    PieVectTable.ADCINT = &adc_isr;
    PieVectTable.XINT1 = &xint1_isr;
    EDIS;

    InitAdc();

    AdcRegs.ADCMAXCONV.all = 0x0000;
    AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0;// ADCINA0
    AdcRegs.ADCTRL2.bit.EXT_SOC_SEQ1 = 1;
    AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1;

    EALLOW;
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0;// LED
    GpioCtrlRegs.GPADIR.bit.GPIO0 = 1;
    EDIS;

    GpioDataRegs.GPASET.bit.GPIO0 = 1;

    EALLOW;
    GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 0;// XINT1
    GpioCtrlRegs.GPADIR.bit.GPIO15 = 0;
    GpioCtrlRegs.GPAPUD.bit.GPIO15 = 1;
    GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 2;
    GpioCtrlRegs.GPACTRL.bit.QUALPRD1 = 0xFF;
    EDIS;

    EALLOW;
    GpioIntRegs.GPIOXINT1SEL.bit.GPIOSEL = 15;
    EDIS;

    XIntruptRegs.XINT1CR.bit.POLARITY = 1;
    XIntruptRegs.XINT1CR.bit.ENABLE = 1;

    PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
    PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
    PieCtrlRegs.PIEIER1.bit.INTx4 = 1;
    IER |= M_INT1;
    EINT;

    for(;;);
    }

    interrupt void adc_isr(void)
    {
    Result = AdcRegs.ADCRESULT0 >>4;

    AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;
    AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
    }

    interrupt void xint1_isr(void)
    {
    GpioDataRegs.GPATOGGLE.bit.GPIO0 = 1;

    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
    }

  • 我已经把程序粘贴到论坛