This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
我在用DRV8301-HC-EVM RevD底板+TMS320F28035板卡调试TI的InstaSPIN-BLDC方案,使用controlSuite里的InstaSPIN-BLDC运行调试,在LEVEL5中,把InstaSPIN_BLDC1.Int_Threshold调低至0.2,此时电机可以从开环启动切入闭环稳定运行,但是当我提高DfuncTesing,也就是提高占空比至0.3时,这时候换向出错,电机停止运行,无论我怎么调Threshold,电机都会在30%~40%这里停止运行,无法提高占空比。
我的 电机是外转子电机,28极,输入电压44V,我是在空载情况下调试的。请问我应该如何调试?您是否有好的建议?谢谢