This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

执行DELAY_US()语句后进入defaultIsr.c中断??

我交替采样两个通道。两个通道采样完毕,下一个循环采样时执行DELAY_US()后进入defaultIsr.c的DATALOG_ISR(),这是为什么?

部分程序:

AdcRegs.ADCTRL2.all=0x2000;

for (;;)

{

while(AdcRegs.ADCST.bit.INT_SEQ1==0)

{}

AdcRegs.ADCST.bit.INT_SEQ1_CLR=1;

SampleTable[array_index++]=((AdcRegs.ADCRESULT0)>>4);

DELAY_US(4000);//the sample rate is 250hz

if (array_index>=1024)

{

。

。

。

}

}

  • 楼主程序是跑在RAM还是FLASH?如果是跑在FLASH里,是否有调用memcpy?芯片是什么型号,楼主可以讲工程放上来,我们分析一下!

  • 我使用CCS3.3对F28335进行烧写,

    该程序的目的是交替对ADCINA0和ADCINB0通道采样,对采集到的信号进行处理。

    该程序未使用中断,利用DELAY_US决定采样率。

    出现问题的语句为DELAY_US(sr_tl)   sr_tl为采样时间间隔

    代码段如下:

    for (;;)

    {

    while(AdcRegs.ADCST.bit.INT_SEQ1==0)

    {}

    AdcRegs.ADCST.bit.INT_SEQ1_CLR=1;

    SampleTable[array_index++]=((AdcRegs.ADCRESULT0)>>4);

    DELAY_US(sr_tl);////the sample rate is 250hz

    if (array_index>=ls)

    {

                        。

                        。//以下是算法部分

                        。

                        。//以下部分是根据算法结果选择ADCINA0或ADCINB0

              if(k_rs==1)

     {

       flag=0;

    AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x08;

    for(index=0;index<ls;index++)

    {

     SampleTable[index]=0;

     }

    }

     if(k_rs==0)

    {

        flag=1;

    AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x00;

    for(index=0;index<ls;index++)

    {

     SampleTable[index]=0;

     }

    }

                                .

                                .

                                .

                       }

           }

    DELAY_US在在第一次交替采样时正常工作,但是在第二次交替采样时出现问题。

    第二次采样到第一个数据点时,执行到DELAY_US后,程序跳到DSP2833x_DefaultIsr.c中去了。

    我单步进入usDelay.asm中,发现在执行SUB ACC,#1后进入DSP2833x_DefaultIsr.c去的。

    进入的是DSP2833x_DefaultIsr.c的以下中断区:

    interrupt void DATALOG_ISR(void)   // Datalogging interrupt

    {

      // Insert ISR Code here

      // Next two lines for debug only to halt the processor here

      // Remove after inserting ISR Code

      asm ("      ESTOP0");

      for(;;);

    }

  • 程序轮廓如下:

    #include "DSP2833x_Device.h"

    #include "DSP2833x_Examples.h"

    #include "math.h"

    。

    。

    。

    。

    void main(void)

    {

    。

    。

    。

    InitSysCtrl();

    // InitXintf();

    InitGpio();////it is important

    InitXintf16Gpio();

    EALLOW;

    SysCtrlRegs.HISPCP.all=ADC_MODCLK;////////clock preset for ADC clock

    EDIS;

    DINT;

    InitPieCtrl();

    IER=0x0000;

    IFR=0x0000;

    InitPieVectTable();

       memcpy(&RamfuncsRunStart,&RamfuncsLoadStart,(&RamfuncsLoadEnd - &RamfuncsLoadStart));

    InitFlash();

    。

    。

    。

    AdcRegs.ADCTRL2.all=0x2000;

    for (;;)

    {

    while(AdcRegs.ADCST.bit.INT_SEQ1==0)

    {}

    AdcRegs.ADCST.bit.INT_SEQ1_CLR=1;

    SampleTable[array_index++]=((AdcRegs.ADCRESULT0)>>4);

    DELAY_US(sr_tl);////the sample rate is 250hz

    if (array_index>=ls)

    {

    。

    。

    。

    }

    }

    }

    F28335的cmd文件:

    MEMORY

    {

    PAGE 0:    /* Program Memory */

              /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

      RAML0       : origin = 0x008000, length = 0x001000     /* on-chip RAM block L0 */  

      FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */

      FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */

      FLASHF      : origin = 0x310000, length = 0x008000     /* on-chip FLASH */

      FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */

      FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */

      FLASHB   : origin = 0x330000, length = 0x008000     /* on-chip FLASH */

      FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */

      CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */

      BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */

      CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */

      OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */

      ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */

      IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */

      IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  

      FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */

      ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        

      RESET       : origin = 0x3FA000, length = 0x000002     /* part of boot ROM  */

      VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

    PAGE 1 :   /* Data Memory */

              /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */

              /* Registers remain on PAGE1                                                  */

      BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */

      RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */

      RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */

      ZONE7       : origin = 0x200000, length = 0x002000

      RAMM2       : origin = 0x009000, length = 0x007000     /* on-chip RAM block L1 */

       FLASHE      : origin = 0x318000, length = 0x008000     /* on-chip FLASH */

    }

    /* Allocate sections to memory blocks.

      Note:

            codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code

                      execution when booting to flash

            ramfuncs  user defined section to store functions that will be copied from Flash into RAM

    */

    SECTIONS

    {

      /* Allocate program areas: */

      .cinit              : > FLASHB      PAGE = 0

      .pinit              : > FLASHB,     PAGE = 0

      .text               : > FLASHB      PAGE = 0

      codestart           : > BEGIN       PAGE = 0

      ramfuncs            : LOAD = FLASHD,

                            RUN = RAML0,

                            LOAD_START(_RamfuncsLoadStart),

                            LOAD_END(_RamfuncsLoadEnd),

                            RUN_START(_RamfuncsRunStart),

                            PAGE=0

      csmpasswds          : > CSM_PWL     PAGE = 0

      csm_rsvd            : > CSM_RSVD    PAGE = 0

      /* Allocate uninitalized data sections: */

      .stack              : > FLASHE       PAGE = 1

      .ebss               : > RAMM2       PAGE = 1

      .esysmem            : > RAMM1       PAGE = 1

      /* Initalized sections go in Flash */

      /* For SDFlash to program these, they must be allocated to page 0 */

      .econst             : > FLASHB      PAGE = 0

      .switch             : > FLASHB      PAGE = 0      

      /* Allocate IQ math areas: */

      IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD

      IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD

      FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

      ZONE7DATA        : > ZONE7        PAGE = 1    

      .reset              : > RESET,      PAGE = 0, TYPE = DSECT

      vectors             : > VECTORS     PAGE = 0, TYPE = DSECT

      /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */

      .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD

    }

    /*

    //===========================================================================

    // End of file.

    //===========================================================================

    */

  • 楼主请将整个项目打包一下传上来,我帮你看一下!

  • 关于DELAY_US问题的真正原因我没有搞清楚。因为它老是跳到中断区,所以我禁止了中断使能,然后使用自己的delay小程序实现了连续采样,目前没有问题。有空我把原来的程序传上来。

  • 你好,Johnson

    这是我写的程序,我运行时,目前程序跑飞到中断区rsvd_isr()

    环境:CCS3.3, F28335, 12864显示屏

    请您帮我看一下,怎么回事?

    请您给我一些建议。

    关于硬件仿真调试我不知道从哪里做起

    谢谢您的帮助

    data acquistion.zip
  • 并且将DELAY_US(stop_df)改为delay(12200)大约为1秒,也出现问题。

  • 楼主,

    你好!

    仿真了一下你的项目确实会跑到ILLEGAL_ISR(void)中断,原因是你的CMD文件堆栈段设置为:

     .stack              : > FLASHE       PAGE = 1

    将其改为如下:

    .stack              : >  RAMM0       PAGE = 1

    同时将链接选项里堆栈大小设为小于0X3B0即可搞定。

    楼主注意堆栈只能放在RAM区,不能放在FLASH区。

  • 非常感谢Johnson的帮助, 现在运行良好!

    你说将堆栈大小设为小于0x3B0,那么堆栈的大小是根据什么设定的?我当初只是随便选择了一个数值,没有任何依据。

  • Johnson,我还有一些问题向您请教。

    在cmd文件中的SECTIONS部分,我对.cinit, .const, .text定义段不是很清晰,我在硬件调试过程中,根据定义段范围我验证了全局变量存储的地址。因此,我有一些疑问。

    就我发给您的程序来说,.

    1. .text  表示可执行代码,存储在FLASHB内

    2. .cinit  它包括初始化的变量和常量表,要求放在程序页,并且在程序开始运行时,C导入路径把数据从.cinit节复制出去然后存在.bss节中。 是不是全局变量初始化值都存在.cinit里面,比较我定义的全局变量 float B_low[3]={...},是不是B_low的内容被存放在.cinit里面?在程度运行时,这些内容会被放入.bss里面相应的地址里?

    3. .pinit   它包括全局构造器(C++)初始化的变量和常量表,要求放在程序页。这个我不懂它指的是什么

    4. .const 或.econst 它包括字符串、声明、以及被明确初始化过的全局和静态变量。我在调试时,发现我定义的字符串str1,str2...都是被存储在PAGE1的RAMM2里面,但是在cmd里面,econst段地址为FLASHB。这是为什么呢?另外为什么我的程序必要要使用econst? 我将econst替换为const, 编译有警告:我没有定义econst.

    5. .bss它为全局变量和静态变量保留空间。这个没有疑问

    6. .esystem动态存储器分配保留空间,这个空间用于外部malloc函数,如果不使用外部malloc函数,这个段的大小就是0,可以放在数据页的任何地方。那么根据我的程序,我不需要定义这个段吧。

    7. .stack为C系统堆栈保留空间。就是我上一问题,根据什么定义堆栈大小

  • 楼主你好.

    1.cinit是用来存放变量初始值的段,在程序复位以后首先会运行_c_int00函数,这个函数会将初始值搬到相应的带初始值的变量。

    2.pinit我的理解是应该在C++时用的,一般用不上!

    3.const 和.econst都是有来存储常量的,主要差异应该是寻址范围,.const是64K范围内,而.econst是全地址范围。

    4..bss和.ebss的差异也是这样,.bss是64K范围内,而.ebss是全地址范围。

    5.esystem这个段的话,如果你没有那些函数的话,也不用管它,有这个段定义它也不会占用RAM空间。

    6..stack大小定义问题,其实要精确定义不太容易,多数时候要靠经验,如果你无法估计它的大小,最简单的办法是给堆栈尽可能的大。至于为什么我将堆栈大小设为小于0X3B0,是因为RAMM0最大只有0X3B0。

  • 楼主,

    你好!

    关于段的含义请参考:TMS320C28x Optimizing C C++ Compiler v6.0.pdf  的第 4.3.6 Specifying Where to Allocate Sections in Memory和第7.1.1 Sections。

    关于堆栈大小定义,其实很难估计准确的堆栈大小,很多情况下靠每个人编程的经验。最简单的办法是给堆栈尽可能的大,这样不容易出现堆栈溢出。至于为什么我说给小于0x3B0,因为0X3B0 是RAMM0的最大长度。

  • 关于stack,我看了汇编方面的内容,不知道是否对dsp通用。8086cpu工作机理为:它是只考虑当前的情况:当前的栈顶在何处,当前要执行的指令是哪一条,而不知道我们安排的栈空间大小。所以无法保证不会栈顶超界。

    那么在程序调试时,如果查看栈空间的出栈入栈情况,在CCS中应该如何操作以便查看?

  • 关于堆栈,汇编和C都是一样的原理,一般来说单片机是无法自身保证堆栈不溢出的,因此需要用户分配足够的空间。当然,这个大小跟程序的结构也有关系,也即跟每个人的编程风格有关,如调的函数层数越大,堆栈自然也要占用更多的空间!

    CCS里面你可以看SP的值。推展占用越多,SP值越大。

  • 此贴  我收获不小啊   谢谢啦

  • 为防止运行过程中堆栈溢出,可以参考文档 Online Stack Overflow Detection on the TMS320C28x DSP 使用在应用程序中加入代码来检测。

    里面的方法同样可以用来检测被意外改写的程序区或数据区。