This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
warning #16002-D: build attribute vendor section TI missing in "../DSP2833x_headers/include/rts2800_eh.lib<boot.obj>": compatibility cannot be determined
error #16008-D: file "../DSP2833x_headers/include/rts2800_eh.lib<boot.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C28FPU32" specified in a previous file or on the command line
error #16019-D: file "../DSP2833x_headers/include/rts2800_eh.lib<boot.obj>" specifies small memory model, which is not compatible with large memory model specified in a previous file or on the command line
warning #16002-D: build attribute vendor section TI missing in "../DSP2833x_headers/include/rts2800_eh.lib<exit.obj>": compatibility cannot be determined
error #16008-D: file "../DSP2833x_headers/include/rts2800_eh.lib<exit.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
error #16019-D: file "../DSP2833x_headers/include/rts2800_eh.lib<exit.obj>" specifies small memory model, which is not compatible with large memory model specified in a previous file or on the command line
warning #16002-D: build attribute vendor section TI missing in "../DSP2833x_headers/include/rts2800_eh.lib<_lock.obj>": compatibility cannot be determined
error #16008-D: file "../DSP2833x_headers/include/rts2800_eh.lib<_lock.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
error #16019-D: file "../DSP2833x_headers/include/rts2800_eh.lib<_lock.obj>" specifies small memory model, which is not compatible with large memory model specified in a previous file or on the command line
您用的TI的例程吗?
建议您烧掉工程中的lib文件,重新添加合适的
可参考帖子:http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/519126?tisearch=e2e-sitesearch&keymatch=specifies%20ISA%20revision%20%22C2800%22