This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助specifies ISA revision "C2800", which is not compatible with ISA revision "C28FPU32" specified in a previous file or on the command line



warning #16002-D: build attribute vendor section TI missing in "../DSP2833x_headers/include/rts2800_eh.lib<boot.obj>": compatibility cannot be determined
error #16008-D: file "../DSP2833x_headers/include/rts2800_eh.lib<boot.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C28FPU32" specified in a previous file or on the command line
error #16019-D: file "../DSP2833x_headers/include/rts2800_eh.lib<boot.obj>" specifies small memory model, which is not compatible with large memory model specified in a previous file or on the command line
warning #16002-D: build attribute vendor section TI missing in "../DSP2833x_headers/include/rts2800_eh.lib<exit.obj>": compatibility cannot be determined
error #16008-D: file "../DSP2833x_headers/include/rts2800_eh.lib<exit.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
error #16019-D: file "../DSP2833x_headers/include/rts2800_eh.lib<exit.obj>" specifies small memory model, which is not compatible with large memory model specified in a previous file or on the command line
warning #16002-D: build attribute vendor section TI missing in "../DSP2833x_headers/include/rts2800_eh.lib<_lock.obj>": compatibility cannot be determined
error #16008-D: file "../DSP2833x_headers/include/rts2800_eh.lib<_lock.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
error #16019-D: file "../DSP2833x_headers/include/rts2800_eh.lib<_lock.obj>" specifies small memory model, which is not compatible with large memory model specified in a previous file or on the command line