This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Code Composer Studio Version: 9.1.0.00010
Emulation package 8.2.0.00004
XDS firmware version :3.0.0.2
DSP:TMS320F280049C
有时一直连接不上DSP:
Error connecting to the target:(Error -260 @ 0x0) An attempt to connect to the XDS110 failed.
能连接时,过大约2-3分钟左右报错:
C28xx_CPU1: JTAG Communication Error: (Error -1135 @ 0x85F4C) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.2.0.00004)
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
你好,我遇到了和你一样的问题。
硬件不动的情况下,使用Flash Programmer 2 将XDS110固件降级后可以正常烧录程序;
再换回ccs9(XDS firmware version :3.0.0.2),就提示-242了。
换了个USB口ccs9就能正常烧录调试。
这感觉像是新的XDS110固件的问题。
我用uniFlash(XDS firmware version :3.0.0.2)和CCS9问题相同。
我是msp432p401r的黑板,当时上机测试直接连的是ccs9.1,应该是强制升级了xds110,而且中间报错了,但现在的情况是我ccs降回了7.4,也安装了flash programmer2,但都显示无法查找到固件,甚至连接usb线后在设备管理器中都无法查看到增加了设备,想问下还有办法解决吗?