Code Composer Studio Version: 9.1.0.00010
Emulation package 8.2.0.00004
XDS firmware version :3.0.0.2
DSP:TMS320F280049C
有时一直连接不上DSP:
Error connecting to the target:(Error -260 @ 0x0) An attempt to connect to the XDS110 failed.
能连接时,过大约2-3分钟左右报错:
C28xx_CPU1: JTAG Communication Error: (Error -1135 @ 0x85F4C) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.2.0.00004)
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging