TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS9.1 XDS110 F280049C调试连接问题

Other Parts Discussed in Thread: TMS320F280049C, UNIFLASH

Code Composer Studio Version: 9.1.0.00010

Emulation package 8.2.0.00004

XDS firmware version :3.0.0.2

DSP:TMS320F280049C

有时一直连接不上DSP:

Error connecting to the target:(Error -260 @ 0x0) An attempt to connect to the XDS110 failed.

能连接时,过大约2-3分钟左右报错:

C28xx_CPU1: JTAG Communication Error: (Error -1135 @ 0x85F4C) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.2.0.00004)

C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

  • 连接一会断开并报错 个人觉得是你的硬件不稳定造成的
    建议先换台电脑 进行测试 如果还是这个情况 建议检查硬件电源 时钟 复位等
  • 我现在使用的也是CCS9.1,连接了280049C Launchpad,测试可以正常连接

    配置如下

    在 TMS320F280049M.ccxml 内,选择2Pin的cjtag

  • 1.检查是不是DSP引脚有虚焊的情况
    2.是不是芯片供电电源松动
  • 调试线缆过长,还有电脑也有问题。
  • 你好,我遇到了和你一样的问题。

    硬件不动的情况下,使用Flash Programmer 2 将XDS110固件降级后可以正常烧录程序;

    再换回ccs9(XDS firmware version :3.0.0.2),就提示-242了。

    换了个USB口ccs9就能正常烧录调试。

    这感觉像是新的XDS110固件的问题。

    我用uniFlash(XDS firmware version :3.0.0.2)和CCS9问题相同。

  • 关于CCS和XDS固件版本问题,有如下描述

    Note that we don’t automatically revert the software unless there’s been a major change. We try to make all changes backwards compatible to ensure this works. If we ever need to make a change that is backwards compatible, then the major version numbers will change as a flag that it can’t work.

    Examples:

    CCS supports firmware 2.3.0.12, XDS110 has firmware 2.3.0.8 → XDS110 will be updated to 2.3.0.12
    CCS supports firmware 2.3.0.12, XDS110 has firmware 2.3.0.14 → XDS110 will not be reverted
    CCS supports firmware 2.3.0.12, XDS110 has firmware 2.4.0.1 → XDS110 will be reverted to 2.3.0.12
  • 我是msp432p401r的黑板,当时上机测试直接连的是ccs9.1,应该是强制升级了xds110,而且中间报错了,但现在的情况是我ccs降回了7.4,也安装了flash programmer2,但都显示无法查找到固件,甚至连接usb线后在设备管理器中都无法查看到增加了设备,想问下还有办法解决吗?