This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp28388D在sci_ex2_loopback_interrupts例程中,为什么SCIA和SCIB可用,配置SCIC和SCID没反应



dsp28388D在sci_ex2_loopback_interrupts例程中,为什么SCIA和SCIB可用,配置SCIC和SCID没反应

  • 能否给出您的相关代码?您的SCIC和SCID的硬件引脚是如何设置的?

  • 用的官方的28388开发板测试,而且是loopback'模式跟管脚没关系
  • 您是否有修改  Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);

    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);

    另外附上我的测试程序,可以成功的

    //###########################################################################
    //
    // FILE:   sci_ex2_loopback_interrupts.c
    //
    // TITLE:  SCI Digital Loop Back with Interrupts.
    //
    //! \addtogroup driver_example_list
    //! <h1> SCI Digital Loop Back with Interrupts </h1>
    //!
    //!  This test uses the internal loop back test mode of the peripheral.
    //!  Other then boot mode pin configuration, no other hardware configuration
    //!  is required. Both interrupts and the SCI FIFOs are used.
    //!
    //!  A stream of data is sent and then compared to the received stream.
    //!  The SCI-A sent data looks like this: \n
    //!  00 01 \n
    //!  01 02 \n
    //!  02 03 \n
    //!  .... \n
    //!  FE FF \n
    //!  FF 00 \n
    //!  etc.. \n
    //!  The pattern is repeated forever.
    //!
    //!  \b Watch \b Variables \n
    //!  - \b sDataA - Data being sent
    //!  - \b rDataA - Data received
    //!  - \b rDataPointA - Keep track of where we are in the data stream.
    //!    This is used to check the incoming data
    //!
    //
    //###########################################################################
    // $TI Release: F2838x Support Library v3.04.00.00 $
    // $Release Date: Fri Feb 12 19:08:49 IST 2021 $
    // $Copyright:
    // Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    
    //
    // Included Files
    //
    #include "driverlib.h"
    #include "device.h"
    
    //
    // Globals
    //
    
    //
    // Send data for SCI-A
    //
    uint16_t sDataA[2];
    
    //
    // Received data for SCI-A
    //
    uint16_t rDataA[2];
    
    //
    // Used for checking the received data
    //
    uint16_t rDataPointA;
    
    //
    // Function Prototypes
    //
    __interrupt void scicTXFIFOISR(void);
    __interrupt void scicRXFIFOISR(void);
    void initSCICFIFO(void);
    void error(void);
    
    //
    // Main
    //
    void main(void)
    {
        uint16_t i;
    
        //
        // Initialize device clock and peripherals
        //
        Device_init();
    
        //
        // Setup GPIO by disabling pin locks and enabling pullups
        //
        Device_initGPIO();
    
        //
        // GPIO28 is the SCI Rx pin.
        //
        GPIO_setMasterCore(39, GPIO_CORE_CPU1);
        GPIO_setPinConfig(GPIO_39_SCIC_RX);
        GPIO_setDirectionMode(39, GPIO_DIR_MODE_IN);
        GPIO_setPadConfig(39, GPIO_PIN_TYPE_STD);
        GPIO_setQualificationMode(39, GPIO_QUAL_ASYNC);
    
        //
        // GPIO29 is the SCI Tx pin.
        //
        GPIO_setMasterCore(38, GPIO_CORE_CPU1);
        GPIO_setPinConfig(GPIO_38_SCIC_TX);
        GPIO_setDirectionMode(38, GPIO_DIR_MODE_OUT);
        GPIO_setPadConfig(38, GPIO_PIN_TYPE_STD);
        GPIO_setQualificationMode(38, GPIO_QUAL_ASYNC);
    
        //
        // Initialize PIE and clear PIE registers. Disables CPU interrupts.
        //
        Interrupt_initModule();
    
        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        //
        Interrupt_initVectorTable();
    
        //
        // Interrupts that are used in this example are re-mapped to
        // ISR functions found within this file.
        //
        Interrupt_register(INT_SCIC_RX, scicRXFIFOISR);
        Interrupt_register(INT_SCIC_TX, scicTXFIFOISR);
    
        //
        // Initialize the Device Peripherals:
        //
        initSCICFIFO();
    
        //
        // Init the send data.  After each transmission this data
        // will be updated for the next transmission
        //
        for(i = 0; i < 2; i++)
        {
            sDataA[i] = i;
        }
    
        rDataPointA = sDataA[0];
    
        Interrupt_enable(INT_SCIC_RX);
        Interrupt_enable(INT_SCIC_TX);
    
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
    
        //
        // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
        //
        EINT;
        ERTM;
    
        //
        // IDLE loop. Just sit and loop forever (optional):
        //
        for(;;);
    }
    
    //
    // error - Function to halt debugger on error
    //
    void error(void)
    {
        asm("     ESTOP0"); // Test failed!! Stop!
        for (;;);
    }
    
    //
    // sciaTXFIFOISR - SCIA Transmit FIFO ISR
    //
    __interrupt void scicTXFIFOISR(void)
    {
        uint16_t i;
    
        SCI_writeCharArray(SCIC_BASE, sDataA, 2);
    
        //
        // Increment send data for next cycle
        //
        for(i = 0; i < 2; i++)
        {
            sDataA[i] = (sDataA[i] + 1) & 0x00FF;
        }
    
        SCI_clearInterruptStatus(SCIC_BASE, SCI_INT_TXFF);
    
        //
        // Issue PIE ACK
        //
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
    }
    
    //
    // sciaRXFIFOISR - SCIA Receive FIFO ISR
    //
    __interrupt void scicRXFIFOISR(void)
    {
        uint16_t i;
    
        SCI_readCharArray(SCIC_BASE, rDataA, 2);
    
        //
        // Check received data
        //
        for(i = 0; i < 2; i++)
        {
            if(rDataA[i] != ((rDataPointA + i) & 0x00FF))
            {
                error();
            }
        }
    
        rDataPointA = (rDataPointA + 1) & 0x00FF;
    
        SCI_clearOverflowStatus(SCIC_BASE);
    
        SCI_clearInterruptStatus(SCIC_BASE, SCI_INT_RXFF);
    
        //
        // Issue PIE ack
        //
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
    }
    
    //
    // initSCIAFIFO - Configure SCIA FIFO
    //
    void initSCICFIFO()
    {
        //
        // 8 char bits, 1 stop bit, no parity. Baud rate is 9600.
        //
        SCI_setConfig(SCIC_BASE, DEVICE_LSPCLK_FREQ, 9600, (SCI_CONFIG_WLEN_8 |
                                                            SCI_CONFIG_STOP_ONE |
                                                            SCI_CONFIG_PAR_NONE));
        SCI_enableModule(SCIC_BASE);
        SCI_enableLoopback(SCIC_BASE);
        SCI_resetChannels(SCIC_BASE);
        SCI_enableFIFO(SCIC_BASE);
    
        //
        // RX and TX FIFO Interrupts Enabled
        //
        SCI_enableInterrupt(SCIC_BASE, (SCI_INT_RXFF | SCI_INT_TXFF));
        SCI_disableInterrupt(SCIC_BASE, SCI_INT_RXERR);
    
        //
        // The transmit FIFO generates an interrupt when FIFO status
        // bits are less than or equal to 2 out of 16 words
        // The receive FIFO generates an interrupt when FIFO status
        // bits are greater than equal to 2 out of 16 words
        //
        SCI_setFIFOInterruptLevel(SCIC_BASE, SCI_FIFO_TX2, SCI_FIFO_RX2);
        SCI_performSoftwareReset(SCIC_BASE);
    
        SCI_resetTxFIFO(SCIC_BASE);
        SCI_resetRxFIFO(SCIC_BASE);
    }
    
    //
    // End of file
    //