This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
speed3.BaseRpm = 120*(BASE_FREQ/POLES);
这个speed3.BaseRpm乘以SpeedRef就是电机的实际转速么
理论上应该是的。建议在英文E2E发帖,请专门的工程师再次确认一下
speed3.BaseRpm这是电机的额定转速 单位是RPM
TI的例程都是归一化的 设定值SpeedRe如果是0.1 就表示设定转速为300RPM
电机转速 = 60 * BASE_FREQ / 电机极对数
如果是8极电机,极对数是4,所以BASE_FREQ = 200Hz
你好,按照你所说的我改了下,电机极对数为5,BASE_FREQ = 250Hz,我给设定值SpeedRef为0.2,可是实际测出的转速为300转,但是滑模观测器估算出的速度为600转,这是什么原因呢
转速=60xF/极对数
根据额定转速 极对数 计算基频 在调试看看
麻烦看下是程序的问题么
我从50Hz的基频调试到200Hz的基频,滑模观测器估算出的转速都为实际转速的2倍