This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: C2Prog烧写程序时报“Bootloading Failed...(invalid echo)”

Part Number: TMS320F28335


各位前辈大家好,我在使用C2prog对TMS320F28335PGFA进行程序烧写时出现报“Bootloading Failed...(invalid echo)”的情况。(我使用的是SCIA接口,能够确保已经进入SCIA引导,烧写方式为RS-422,波特率9600,板卡晶振为10MHz)

对同样的多张板卡进行烧写时,有40%左右的板卡会出现这个故障。我对出现故障的板卡更换CPU芯片后,又能够正常写入了。但是我觉得应该不是芯片自身的问题。大家觉得有什么可能性导致这个故障的故障率这么高。

有没有什么方法能够提高C2porg对28335的烧写成功率啊,总不能写不进就换CPU,成本扛不住。。。。

感谢~

如图