This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位前辈大家好,我在使用C2prog对TMS320F28335PGFA进行程序烧写时出现报“Bootloading Failed...(invalid echo)”的情况。(我使用的是SCIA接口,能够确保已经进入SCIA引导,烧写方式为RS-422,波特率9600,板卡晶振为10MHz)
对同样的多张板卡进行烧写时,有40%左右的板卡会出现这个故障。我对出现故障的板卡更换CPU芯片后,又能够正常写入了。但是我觉得应该不是芯片自身的问题。大家觉得有什么可能性导致这个故障的故障率这么高。
有没有什么方法能够提高C2porg对28335的烧写成功率啊,总不能写不进就换CPU,成本扛不住。。。。
感谢~
如图
请问能否给出您的相关配置截图?Bootloading… failed (invalid echo)!一般是返回值不对,请问在不bootload时候,SCI通信正常?您的hex文件生成格式是否正确,为intel hex格式?
另外您是在何处购买的芯片?
还是要固定选择为30MHz啊。
据我所知是需要固定的30MHz
最后面,多收到了00 00,请问是什么原因呢?
这个确实有些奇怪,是发送特定字符串才会多出00还是无论发送什么都会有这样的现象?