TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: IPC例程问题

Part Number: TMS320F28388D

例程是单次发送且CPU没有接收中断,在while中连续发送不好使

参考历程ipc_ex2_msgqueue_cm

  • IPC_readMessageFromQueue()

    IPC_readCommand()

    两者什么区别

  • CPU如何加接收中断,目前测试CPU发送-接收-发送,第二次发送后Cm就无法进中断

  • 您可以看一下 ipc.h内的函数说明

    一个是read message,一个是read command

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    //*****************************************************************************
    //
    //! Reads a message from the messageQueue.
    //!
    //! \param ipcType is the enum corresponding to the IPC instance used
    //! \param msgQueue specifies the address of a \e IPC_MessageQueue_t instance
    //! \param addrCorrEnable is the flag used to determine whether or not to
    //! convert the addr parameter to remote core's address space
    //! \param msg specifies the address of the \e IPC_Message_t instance to which
    //! the message needs to be read
    //! \param block specifies whether to allow function to block until a message
    //! is available in the message queue
    //!
    //! This function checks if there is a message in the message queue. If so, it
    //! reads the message and writes to the address pointed to by \e msg into.
    //!
    //! The \e addrCorrEnable parameter can take values IPC_ADDR_CORRECTION_ENABLE
    //! (converts the address to remote core's address space) or
    //! IPC_ADDR_CORRECTION_DISABLE(does not modify the addr parmeter)
    //! The \e block parameter can be one of the following values:
    //! \b IPC_BLOCKING_CALL or \b IPC_NONBLOCKING_CALL.
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    //*****************************************************************************
    //
    //! Reads a command sent by the Remote core
    //!
    //! \param ipcType is the enum corresponding to the IPC instance used
    //! \param flags is the IPC flag mask for the flags sent by the remote core
    //! \param addrCorrEnable is the flag used to determine whether or not to
    //! convert the addr parameter to remote core's address space
    //! \param command is the 32-bit pointer at which the command value is read to
    //! \param addr is the 32-bit pointer at which address value is read to
    //! \param data is the 32-bit pointer at which the data is read to
    //!
    //! Allows the caller to read a command sent by the remote core. A command
    //! consists of a unique command value, a 32-bit address and a 32-bit data.
    //! There may be differences in the address spaces of Local and Remote core.
    //! For example in case of F2838X device, the address spaces of C28x core and
    //! CM core are different. In case the \e addr refers to an address in the IPC
    //! MSG RAM, \e addrCorrEnable param may be used to correct the address mismatch
    //!
    //! The \e flags parameter can be any of the IPC flag values: \b IPC_FLAG0 -
    //! \b IPC_FLAG31.
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • CPU如何加接收中断

    在英文E2E上有相关讨论,您可以先看一下

    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/891832/ccs-tms320f28388d-how-to-trigger-ipc-interrupt-in-cpu1 

    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/852116/tms320f28388d-how-to-trigger-interrupt-by-sending-ipc-message-cm-to-cpu1 

    若还是不能成功,请您再次回复,并附上代码

  • //#############################################################################
    //
    // FILE: ethernet_ipc_ex1_basic_c28x1.c
    //
    // TITLE: Ethernet IPC example with interrupt
    //
    //! \addtogroup driver_cm_c28x_dual_example_list
    //! <h1> Ethernet + IPC basic message passing example with interrupt </h1>
    //!
    //! This example demonstrates how to configure IPC and pass information from
    //! C28x to CM core without message queues. This configures the Pinmux for Ethernet
    //! Prepares the Ethernet frame that is sent to the CM core
    //! over IPC Message RAM. Uses the IPC command interface to signal
    //! the IPC Command, Packet address, Packet Length which is used by CM
    //! side code to send it on the Ethernet Line, which is acknowledged by
    //! the CM core side code over IPC on succesfully receiving a packet
    //! It is recommended to run the C28x1 core first, followed by the CM core.
    //!
    //! \b External \b Connections \n
    //! - Connections for Ethernet in MII mode
    //!
    //! \b Watch \b Variables \n
    //! - pass
    //!
    //
    //#############################################################################
    // $TI Release: F2838x Support Library v3.03.00.00 $
    // $Release Date: Sun Oct 4 16:00:36 IST 2020 $
    // $Copyright:
    // Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without
    // modification, are permitted provided that the following conditions
    // are met:
    //
    // Redistributions of source code must retain the above copyright
    // notice, this list of conditions and the following disclaimer.
    //
    // Redistributions in binary form must reproduce the above copyright
    // notice, this list of conditions and the following disclaimer in the
    // documentation and/or other materials provided with the
    // distribution.
    //
    // Neither the name of Texas Instruments Incorporated nor the names of
    // its contributors may be used to endorse or promote products derived
    // from this software without specific prior written permission.
    //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################

    //
    // Included Files
    //
    #include "driverlib.h"
    #include "device.h"

    //
    // Defines
    //
    #define IPC_CMD_READ_MEM 0x1001
    #define IPC_CMD_RESP 0x2001

    #define TEST_PASS 0x5555
    #define TEST_FAIL 0xAAAA

    #define PACKET_LENGTH 132
    #pragma DATA_SECTION(packetData, "MSGRAM_CPU_TO_CM")
    uint8_t packetData[PACKET_LENGTH];

    uint32_t pass;
    uint16_t count,countpr;
    uint32_t command, addr, data;
    void IPC_ISR0()
    {


    IPC_readCommand(IPC_CPU1_L_CM_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
    &command, &addr, &data);

    IPC_ackFlagRtoL(IPC_CPU1_L_CM_R, IPC_FLAG0);

    // IPC_sendResponse(IPC_CPU1_L_CM_R, TEST_PASS);

    count++;

    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP11);
    }
    //
    void main(void)
    {
    int i;

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    Interrupt_initModule();
    Interrupt_initVectorTable();

    //
    // Boot CM core
    //
    #ifdef _FLASH
    Device_bootCM(BOOTMODE_BOOT_TO_FLASH_SECTOR0);
    #else
    Device_bootCM(BOOTMODE_BOOT_TO_S0RAM);
    #endif


    //
    // Clear any IPC flags if set already
    //
    IPC_clearFlagLtoR(IPC_CPU1_L_CM_R, IPC_FLAG_ALL);

    IPC_registerInterrupt(IPC_CPU1_L_CM_R, IPC_INT0, IPC_ISR0);
    // Synchronize both the cores.
    //
    IPC_sync(IPC_CPU1_L_CM_R, IPC_FLAG31);

    Interrupt_enable(INT_CMTOCPUXIPC0);

    EINT;
    ERTM;


    //
    // Send a message without message queue
    // Since C28x and CM does not share the same address space for shared RAM,
    // ADDRESS_CORRECTION is enabled
    // Length of the data to be read is passed as data.
    //
    IPC_sendCommand(IPC_CPU1_L_CM_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
    IPC_CMD_READ_MEM, (uint32_t)packetData, PACKET_LENGTH);

    //
    // Wait for acknowledgment
    //
    // IPC_waitForAck(IPC_CPU1_L_CM_R, IPC_FLAG0);

    while(1)
    {
    if(count!=countpr)
    {
    countpr = count;
    IPC_sendCommand(IPC_CPU1_L_CM_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
    IPC_CMD_READ_MEM, (uint32_t)packetData, PACKET_LENGTH);

    }
    }
    }
    //
    // End of File
    //


  • //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################

    //
    // Included Files
    //
    #include "driverlib_cm.h"

    //
    // Defines
    //
    #define IPC_CMD_READ_MEM 0x1001
    #define IPC_CMD_RESP 0x2001

    #define TEST_PASS 0x5555
    #define TEST_FAIL 0xAAAA

    //
    // Defines
    //
    #define PACKET_LENGTH 132


    #define ETHERNET_NO_OF_RX_PACKETS 1U
    //
    //Change this define for changing Packet buffer length
    //
    #define ETHERNET_MAX_PACKET_LENGTH 1538U
    uint16_t count;


    //
    // Globals
    //
    uint8_t pData[PACKET_LENGTH];
    uint8_t Ethernet_rxBuffer[ETHERNET_NO_OF_RX_PACKETS *
    ETHERNET_MAX_PACKET_LENGTH];
    Ethernet_Handle emac_handle;
    Ethernet_Pkt_Desc pktDesc;
    extern uint32_t Ethernet_rxInterruptCount;
    bool status = false;

    uint32_t command, addr, data;
    // IPC ISR for Flag 0.
    // C28x core sends data without message queue using Flag 0
    uint8_t packetData[PACKET_LENGTH];
    void IPC_ISR0()
    {


    IPC_readCommand(IPC_CM_L_CPU1_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
    &command, &addr, &data);

    IPC_sendResponse(IPC_CM_L_CPU1_R, TEST_PASS);
    IPC_sendCommand(IPC_CM_L_CPU1_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
    IPC_CMD_READ_MEM, (uint32_t)packetData, PACKET_LENGTH);
    IPC_ackFlagRtoL(IPC_CM_L_CPU1_R, IPC_FLAG0);
    count++;
    }


    void main(void)
    {

    //
    // Clear any IPC flags if set already
    //
    IPC_clearFlagLtoR(IPC_CM_L_CPU1_R, IPC_FLAG_ALL);

    //
    // Enable IPC interrupts
    //
    IPC_registerInterrupt(IPC_CM_L_CPU1_R, IPC_INT0, IPC_ISR0);

    //
    // Synchronize both the cores.
    //
    IPC_sync(IPC_CM_L_CPU1_R, IPC_FLAG31);



    //
    //The control data to C28x side can be picked up from Ethernet buffer and
    //Passed to Ethernet
    //
    // Send response to C28x core
    //
    // if(status)
    // {
    // IPC_sendResponse(IPC_CM_L_CPU1_R, TEST_PASS);
    // }
    // else
    // {
    // IPC_sendResponse(IPC_CM_L_CPU1_R, TEST_FAIL);
    // }

    //
    // Acknowledge the flag
    //

    // IPC_sendCommand(IPC_CM_L_CPU1_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
    // IPC_CMD_READ_MEM, (uint32_t)packetData, PACKET_LENGTH);
    // __asm(" bkpt #0");
    while(1)
    {
    if(IPC_getResponse(IPC_CM_L_CPU1_R) == TEST_PASS)
    {

    // IPC_sendCommand(IPC_CM_L_CPU1_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
    // IPC_CMD_READ_MEM, (uint32_t)packetData, PACKET_LENGTH);
    // count=0;
    }

    }

    }
    //
    // End of File
    //

  • 目前问题:cm进中断后发送数据,CPU接收后进入中断出中断程序跑飞,在线复位都不行

  • 请您之后以 “插入-->代码” 的形式来上传代码

    cm进中断后发送数据,CPU接收后进入中断出中断程序跑飞

    是否有查看对应的标志位?

  • Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    //#############################################################################
    //
    // FILE: ethernet_ipc_ex1_basic_c28x1.c
    //
    // TITLE: Ethernet IPC example with interrupt
    //
    //! \addtogroup driver_cm_c28x_dual_example_list
    //! <h1> Ethernet + IPC basic message passing example with interrupt </h1>
    //!
    //! This example demonstrates how to configure IPC and pass information from
    //! C28x to CM core without message queues. This configures the Pinmux for Ethernet
    //! Prepares the Ethernet frame that is sent to the CM core
    //! over IPC Message RAM. Uses the IPC command interface to signal
    //! the IPC Command, Packet address, Packet Length which is used by CM
    //! side code to send it on the Ethernet Line, which is acknowledged by
    //! the CM core side code over IPC on succesfully receiving a packet
    //! It is recommended to run the C28x1 core first, followed by the CM core.
    //!
    //! \b External \b Connections \n
    //! - Connections for Ethernet in MII mode
    //!
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX
    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    //
    // Included Files
    //
    #include "driverlib_cm.h"
    //
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • 帮看一下CPU的IPC中断到底怎么搞,很着急。谢谢

  • CM中    IPC_registerInterrupt(IPC_CM_L_CPU1_R, IPC_INT0, IPC_ISR0);为什么IPC_INT0能进入其他不行,没有看到在何使能中断

  • 1 CM中的代码没有改变

    2 CPU1内的代码如下 

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    //#############################################################################
    //
    // FILE: ipc_ex2_msgqueue_c28x1.c
    //
    // TITLE: IPC example with interrupt and message queue
    //
    //! \addtogroup driver_cm_c28x_dual_example_list
    //! <h1> IPC message passing example with interrupt and message queue </h1>
    //!
    //! This example demonstrates how to configure IPC and pass information from
    //! C28x to CM core with message queues.
    //! It is recommended to run the C28x1 core first, followed by the CM core.
    //!
    //! \b External \b Connections \n
    //! - None.
    //!
    //! \b Watch \b Variables \n
    //! - pass
    //!
    //
    //#############################################################################
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX