我在使用CLA的过程中发现
CLA的初始化如下
void CLLLC_HAL_setupCLA(void)
{
//
// setup CLA to register an interrupt
//
#if CLLLC_ISR1_RUNNING_ON == CLA_CORE
memcpy((uint32_t *)&Cla1ProgRunStart, (uint32_t *)&Cla1ProgLoadStart,
(uint32_t)&Cla1ProgLoadSize );
//
// first assign memory to CLA
//
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS0, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS1, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS2, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS3, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS4, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS5, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS6, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS7, MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS0, MEMCFG_CLA_MEM_DATA);
MemCfg_setCLAMemType(MEMCFG_SECT_LS1, MEMCFG_CLA_MEM_DATA);
MemCfg_setCLAMemType(MEMCFG_SECT_LS2, MEMCFG_CLA_MEM_DATA);
MemCfg_setCLAMemType(MEMCFG_SECT_LS3, MEMCFG_CLA_MEM_DATA);
MemCfg_setCLAMemType(MEMCFG_SECT_LS4, MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setCLAMemType(MEMCFG_SECT_LS5, MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setCLAMemType(MEMCFG_SECT_LS6, MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setCLAMemType(MEMCFG_SECT_LS7, MEMCFG_CLA_MEM_PROGRAM);
//
// Suppressing #770-D conversion from pointer to smaller integer
// The CLA address range is 16 bits so the addresses passed to the MVECT
// registers will be in the lower 64KW address space. Turn the warning
// back on after the MVECTs are assigned addresses
//
#pragma diag_suppress = 770
CLA_mapTaskVector(CLA1_BASE , CLA_MVECT_1, (uint16_t)&Cla1Task1);
CLA_mapTaskVector(CLA1_BASE , CLA_MVECT_2, (uint16_t)&Cla1Task2);
CLA_mapTaskVector(CLA1_BASE , CLA_MVECT_3, (uint16_t)&Cla1Task3);
CLA_mapTaskVector(CLA1_BASE , CLA_MVECT_4, (uint16_t)&Cla1Task4);
CLA_mapTaskVector(CLA1_BASE , CLA_MVECT_5, (uint16_t)&Cla1Task5);
CLA_mapTaskVector(CLA1_BASE , CLA_MVECT_6, (uint16_t)&Cla1Task6);
CLA_mapTaskVector(CLA1_BASE , CLA_MVECT_7, (uint16_t)&Cla1Task7);
CLA_mapBackgroundTaskVector(CLA1_BASE, (uint16_t)&Cla1BackgroundTask);
#pragma diag_warning = 770
CLA_enableIACK(CLA1_BASE);
CLA_enableTasks(CLA1_BASE, CLA_TASKFLAG_ALL);
CLA_enableHardwareTrigger(CLA1_BASE);
CLA_setTriggerSource(CLA_TASK_8, CLLLC_ISR2_TRIG_CLA);
CLA_enableBackgroundTask(CLA1_BASE);
CLA_setTriggerSource(CLA_TASK_1, CLLLC_ISR2_TRIG_CLA);//CLA_TRIGGER_ADCB1);//CLLLC_ISR1_TRIG_CLA);
#endif
}
当我使用BackgroundTask时
__attribute__((interrupt("background"))) void Cla1BackgroundTask ( void )
{
#ifdef BUCK_CONTROL_RUNNING_ON_CLA
BUCK_runIsr();
#ifdef BUCK2_ENABLE
BUCK2_runIsr();
#endif
#ifdef BUCK3_ENABLE
BUCK3_runIsr();
#endif
#ifdef BUCK4_ENABLE
BUCK4_runIsr();
#endif
#endif
if(CLAtest == 1)
{
CLLLC_HAL_setProfilingGPIO2();//GPIO22置高
CLAtest = 0;
}
else
{
CLLLC_HAL_resetProfilingGPIO2();//GPIO22置低
CLAtest = 1;
}
}
编译就会不通过,如图

但当我把相同的任务内容放在Task1时
__attribute__((interrupt)) void Cla1Task1 ( void )
{
#if(CLA_DEBUG == 1)
__mdebugstop();
#endif
#ifdef BUCK_CONTROL_RUNNING_ON_CLA
BUCK_runIsr();
#ifdef BUCK2_ENABLE
BUCK2_runIsr();
#endif
#ifdef BUCK3_ENABLE
BUCK3_runIsr();
#endif
#ifdef BUCK4_ENABLE
BUCK4_runIsr();
#endif
#endif
if(CLAtest == 1)
{
CLLLC_HAL_setProfilingGPIO2();//GPIO22置高
CLAtest = 0;
}
else
{
CLLLC_HAL_resetProfilingGPIO2();//GPIO22置低
CLAtest = 1;
}
}
程序就能编译通过并正常运行,这是什么原因?