This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在是28335读FPGA的数据:
可以看到XRD和XWE 的同时拉低,但手册里说这两条线是互斥的,所以现在很疑惑出现这个状态!
下面是我Xintf的初始化的代码
void init_zone7(void) { // // Make sure the XINTF clock is enabled // EALLOW; SysCtrlRegs.PCLKCR3.bit.XINTFENCLK = 1; EDIS; // // Configure the GPIO for XINTF with a 16-bit data bus // This function is in DSP2833x_Xintf.c // InitXintf16Gpio(); EALLOW; // // All Zones // Timing for all zones based on XTIMCLK = SYSCLKOUT/2 // XintfRegs.XINTCNF2.bit.XTIMCLK = 1; // // Buffer up to 0 writes // XintfRegs.XINTCNF2.bit.WRBUFF = 0; // // XCLKOUT is enabled // XintfRegs.XINTCNF2.bit.CLKOFF = 0; // // XCLKOUT = XTIMCLK // XintfRegs.XINTCNF2.bit.CLKMODE = 0; // // Enable XHOLD to prevent XINTF bus from going into high impedance state // whenever TZ3 signal goes low. This occurs because TZ3 on GPIO14 is // shared with HOLD of XINTF // XintfRegs.XINTCNF2.bit.HOLD = 1; // // Zone 7 // When using ready, ACTIVE must be 1 or greater. Lead must always be 1 or // greater. Zone write timing // XintfRegs.XTIMING7.bit.XWRLEAD = 2; XintfRegs.XTIMING7.bit.XWRACTIVE = 4; XintfRegs.XTIMING7.bit.XWRTRAIL = 2; // // Zone read timing // XintfRegs.XTIMING7.bit.XRDLEAD = 2; XintfRegs.XTIMING7.bit.XRDACTIVE = 6; XintfRegs.XTIMING7.bit.XRDTRAIL = 0; // // don't double all Zone read/write lead/active/trail timing // XintfRegs.XTIMING7.bit.X2TIMING = 1; // // Zone will sample XREADY signal // XintfRegs.XTIMING7.bit.USEREADY = 1; XintfRegs.XTIMING7.bit.READYMODE = 0; // // 1,1 = x16 data bus // 0,1 = x32 data bus // other values are reserved // XintfRegs.XTIMING7.bit.XSIZE = 3; // Bank switching // Assume Zone 7 is slow, so add additional BCYC cycles // when ever switching from Zone 7 to another Zone. // This will help avoid bus contention. XintfRegs.XBANK.bit.BANK = 7; XintfRegs.XBANK.bit.BCYC = 7; EDIS; // // // // // Force a pipeline flush to ensure that the write to // // the last register configured occurs before returning. // // // __asm(" RPT #7 || NOP"); }
下面是我读数据的代码
for ( i = 0; i < 2048; i++) { /* code */ *(DSP_Buf+i) = *(FPGA_RamStart+i); }
你好,不知道图片中的是XWE0还是XWE1?与XRD互斥的只是XWE0
The XRD and XWE0 signals are mutually exclusive.
另外,关键是你的代码运行后能正常访问FPGA吗?
可以共享执行代码和“DSP_Buf”的内存地址吗?程序是从芯片内部ram或者flash启动的吗?
从代码看,WE应该不是active的吧?