This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题:现有一批TMS320LF2406A需要烧录.out程序。我目前使用虚拟机安装了XP系统,安装ccs3.3版本,使用的是XDS510仿真器。
仿真器驱动安装应该没有问题,设备管理器中可以正常识别。如下图:
在点击setupccstudio后配置如下:
点击保存同时打开ccs,弹出如下错误:
芯片型号选择其他型号:如F28335 XDS510则不会出现此错误。
1、麻烦问下怎么解决这个问题。网上有说安装 SR12_CCS_v3.3_SR_3.3.82.13.exe可以解决,但是重新安装了几遍还是一样的问题。
2,我查了可以使用串口进行下载,我用了C2Prog V1.9版本,选择了.out烧录文件,点击program,程序没有任何报错,直接退出了。
3,是否还有其他简单点的烧录办法?
使用C2prog V1.9版本,选择了.hex烧录文件,在pinging target的时候显示no response,麻烦问下2406进入SCI BOOT模式是只需要把BOOT_EN引脚拉低就可以了吗?
补充说明:更换为ccs3.1,不再出现此错误。但是出现新的问题:点击load progam 报错:
one or more sections of your program falls into a memory region that is not writable
额,很抱歉这款芯片是真的没有用过,包括CCS3.3也是好几年没用,真说不上什么建议了。
不过CCS3.1的报错,是不是跟你的cmd文件内存分配有关?或者target configuration的配置有关?