This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28335 I2C



最近需要用28335读I2C的气压计,初始化I2C为:

I2caRegs.I2CMDR.bit.IRS =0;    I2caRegs.I2CSAR = 0x0050;  // Slave address - EEPROM control code   

I2caRegs.I2CPSC.all = 15;   // Prescaler - need 7-12 Mhz on module clk   

I2caRegs.I2CCLKL = 15;   // NOTE: must be non zero   

I2caRegs.I2CCLKH = 15;   // NOTE: must be non zero   

I2caRegs.I2CIER.all = 0x00;  // Enable SCD & ARDY interrupts

I2caRegs.I2CMDR.bit.IRS = 1; // Take I2C out of reset

写程序:

Uint16 WriteData(Uint16 Address) {  

  Uint16 i;    if (I2caRegs.I2CSTR.bit.BB == 1)    {       return I2C_BUS_BUSY_ERROR;    }   

 while(!I2C_xrdy());   

 I2caRegs.I2CSAR = 0x1E;   

 I2caRegs.I2CCNT = 1;   

I2caRegs.I2CDXR = Address;   

I2caRegs.I2CMDR.all = 0x6E20;        

 if (I2caRegs.I2CSTR.bit.NACK == 1)     

  return I2C_BUS_BUSY_ERROR;     

 return I2C_SUCCESS;   }

为什么我在主程序中调用 WriteData(0X1E),用示波器看引脚波形,发现什么都没有,是什么情况?求指导~