Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
- 目标:是通过SYS/BIOS System Analyzer功能 查看Task HWI SWI 的实际运行性能;
用的各软件版本如下:
|
CCS |
CCS v11.1.0.00011 |
|
编译器 |
C2000 Compiler v21.12.0.STS |
|
XDCtools |
XDCtools v3.62.1.16.core |
|
SYS/BIOS |
SYS/BIOS v6.83.0.18 |
|
UIA |
uia_2_30_01_02 |
|
Target |
ti.targets.C28_float |
- 异常现象如下:




02.01. Error: Failed to start ROV using 'comm=DSLite:0,wsPort=58037':InternalError: Can't find method xdc.rta.Formatter.setOFReader(org.mozilla.javascript.Undefined). (C:/ti/ccs1110/xdctools_3_62_01_16_core/packages/xdc/rov/Model.xs#315)
02.02.
Received exception from ROV:server Target memory read failed at address :0x04, length :26,This read is an
INVALID address according to the application's section map .The application is likely either unintialized or corrupt.