This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用的各软件版本如下:
CCS |
CCS v11.1.0.00011 |
编译器 |
C2000 Compiler v21.12.0.STS |
XDCtools |
XDCtools v3.62.1.16.core |
SYS/BIOS |
SYS/BIOS v6.83.0.18 |
UIA |
uia_2_30_01_02 |
Target |
ti.targets.C28_float |
02.01. Error: Failed to start ROV using 'comm=DSLite:0,wsPort=58037':InternalError: Can't find method xdc.rta.Formatter.setOFReader(org.mozilla.javascript.Undefined). (C:/ti/ccs1110/xdctools_3_62_01_16_core/packages/xdc/rov/Model.xs#315)
02.02.
Received exception from ROV:server Target memory read failed at address :0x04, length :26,This read is an
INVALID address according to the application's section map .The application is likely either unintialized or corrupt.
你好,
上图中的错误是什么时候出现的?是在代码运行之前吗?如果是的话,那我认为是正常的——看下下面这个链接:
ROV BIOS Scan for Errors 该界面显示有错误吗?
这个地址应该是在boot ROM中的wait boot,你可以通过加载这些标志来检查:
[c2000ware installation]\libraries\boot_rom\f2837xs\revB\rom_sources\ccs_files\cpu01\Release\F2837x_cpu01_bootROM_REVB_Golden_020314.out
然后再Locate file 中填入:[c2000ware installation]]\libraries\boot_rom\f2837xs\revB\rom_sources\F2837x_bootROM\cpu01-bootROM\source
然后你应该可以看到在boot ROM中的停止位置。不管怎样,有什么东西导致了重置。你能检查复位原因寄存器吗?
澄清一下,我是在问 BIOS 部分中 ROV 中的“scan for errors”。