This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: SYS/BIOS System Analyzer:01. ROVcan not load no symbles and program ; 02. LoggerStopMode Target memory read failed

Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
  1. 目标:是通过SYS/BIOS  System Analyzer功能 查看Task HWI SWI 的实际运行性能;

用的各软件版本如下:

CCS 

CCS v11.1.0.00011

编译器

C2000 Compiler v21.12.0.STS

XDCtools 

XDCtools v3.62.1.16.core

SYS/BIOS 

SYS/BIOS v6.83.0.18

UIA

uia_2_30_01_02

Target

ti.targets.C28_float

  1. 异常现象如下:

02.01. Error: Failed to start ROV using 'comm=DSLite:0,wsPort=58037':InternalError: Can't find method xdc.rta.Formatter.setOFReader(org.mozilla.javascript.Undefined). (C:/ti/ccs1110/xdctools_3_62_01_16_core/packages/xdc/rov/Model.xs#315) 

 

02.02.

Received exception from ROV:server Target memory read failed at address :0x04, length :26,This read is an 

INVALID address according to the application's section map .The application is likely either unintialized or corrupt.