This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: CAN的波特率寄存器无法写入

Part Number: TMS320F2800137
Other Parts Discussed in Thread: C2000WARE, ISO1050

我使用的开发版本是CCS12版本。使用的是官网上的demo板。根据官网提供的例程进行操作,在初始化 芯片和GPIO引脚之后,进行CAN模块的配置,发现CAN_BTR寄存 器无法写入。而CAN_CTL寄存器也无法也有一些位无法操作,比如说CCE位,该位应该在CAN_initModule()函数里面就调用了。我这边以为是CAN时钟无法配置导致的,但是在Device_init()之后,可以看到 CAN的外设时钟已经打开。还有一个是,尝试过,直接操作CAN_BTR也无法操作