This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为内存不够就把 28033_RAM_lnk.cmd修改了一下,结果DSP2803x_Headers_nonBIOS.cmd就报了这个错误:#10264 PARTID memory range。
28033_RAM_lnk.cmd文件如下。我主要是把RAML0L1改大了。
MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x000000, length = 0x000002 RAMM0 : origin = 0x000050, length = 0x0003B0 RAML0L1 : origin = 0x000800, length = 0x2F3F00 RESET : origin = 0x3FFFC0, length = 0x000002 IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ BOOTROM : origin = 0x3FF27C, length = 0x000D44 PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x00004E /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000480, length = 0x000380 /* on-chip RAM block M1 */ RAML2 : origin = 0x2F4700, length = 0x100450 RAML3 : origin = 0x3F4B50, length = 0x001000 } SECTIONS { /* Setup for "boot to SARAM" mode: The codestart section (found in DSP28_CodeStartBranch.asm) re-directs execution to the start of user code. */ codestart : > BEGIN, PAGE = 0 ramfuncs : > RAMM0 PAGE = 0 .text : > RAML0L1, PAGE = 0 .cinit : > RAMM0, PAGE = 0 .pinit : > RAMM0, PAGE = 0 .switch : > RAMM0, PAGE = 0 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ .stack : > RAMM1, PAGE = 1 .ebss : > RAML2, PAGE = 1 .econst : > RAML2, PAGE = 1 .esysmem : > RAML2, PAGE = 1 IQmath : > RAML0L1, PAGE = 0 IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD }
DSP2803x_Headers_nonBIOS.cmd我没有过。
MEMORY { PAGE 0: /* Program Memory */ PAGE 1: /* Data Memory */ DEV_EMU : origin = 0x000880, length = 0x000105 /* device emulation registers */ SYS_PWR_CTL : origin = 0x000985, length = 0x000003 /* System power control registers */ FLASH_REGS : origin = 0x000A80, length = 0x000060 /* FLASH registers */ CSM : origin = 0x000AE0, length = 0x000010 /* code security module registers */ ADC_RESULT : origin = 0x000B00, length = 0x000020 /* ADC Results register mirror */ CPU_TIMER0 : origin = 0x000C00, length = 0x000008 /* CPU Timer0 registers */ CPU_TIMER1 : origin = 0x000C08, length = 0x000008 /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/ CPU_TIMER2 : origin = 0x000C10, length = 0x000008 /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/ PIE_CTRL : origin = 0x000CE0, length = 0x000020 /* PIE control registers */ PIE_VECT : origin = 0x000D00, length = 0x000100 /* PIE Vector Table */ CLA1 : origin = 0x001400, length = 0x000080 /* CLA registers */ ECANA : origin = 0x006000, length = 0x000040 /* eCAN-A control and status registers */ ECANA_LAM : origin = 0x006040, length = 0x000040 /* eCAN-A local acceptance masks */ ECANA_MOTS : origin = 0x006080, length = 0x000040 /* eCAN-A message object time stamps */ ECANA_MOTO : origin = 0x0060C0, length = 0x000040 /* eCAN-A object time-out registers */ ECANA_MBOX : origin = 0x006100, length = 0x000100 /* eCAN-A mailboxes */ COMP1 : origin = 0x006400, length = 0x000020 /* Comparator + DAC 1 registers */ COMP2 : origin = 0x006420, length = 0x000020 /* Comparator + DAC 2 registers */ COMP3 : origin = 0x006440, length = 0x000020 /* Comparator + DAC 3 registers */ EPWM1 : origin = 0x006800, length = 0x000040 /* Enhanced PWM 1 registers */ EPWM2 : origin = 0x006840, length = 0x000040 /* Enhanced PWM 2 registers */ EPWM3 : origin = 0x006880, length = 0x000040 /* Enhanced PWM 3 registers */ EPWM4 : origin = 0x0068C0, length = 0x000040 /* Enhanced PWM 4 registers */ EPWM5 : origin = 0x006900, length = 0x000040 /* Enhanced PWM 5 registers */ EPWM6 : origin = 0x006940, length = 0x000040 /* Enhanced PWM 6 registers */ EPWM7 : origin = 0x006980, length = 0x000040 /* Enhanced PWM 7 registers */ ECAP1 : origin = 0x006A00, length = 0x000020 /* Enhanced Capture 1 registers */ HRCAP1 : origin = 0x006AC0, length = 0x000020 /* High Resolution Capture 1 registers */ HRCAP2 : origin = 0x006AE0, length = 0x000020 /* High Resolution Capture 2 registers */ EQEP1 : origin = 0x006B00, length = 0x000040 /* Enhanced QEP 1 registers */ LINA : origin = 0x006C00, length = 0x000080 /* LIN-A registers */ GPIOCTRL : origin = 0x006F80, length = 0x000040 /* GPIO control registers */ GPIODAT : origin = 0x006FC0, length = 0x000020 /* GPIO data registers */ GPIOINT : origin = 0x006FE0, length = 0x000020 /* GPIO interrupt/LPM registers */ SYSTEM : origin = 0x007010, length = 0x000020 /* System control registers */ SPIA : origin = 0x007040, length = 0x000010 /* SPI-A registers */ SPIB : origin = 0x007740, length = 0x000010 /* SPI-B registers */ SCIA : origin = 0x007050, length = 0x000010 /* SCI-A registers */ NMIINTRUPT : origin = 0x007060, length = 0x000010 /* NMI Watchdog Interrupt Registers */ XINTRUPT : origin = 0x007070, length = 0x000010 /* external interrupt registers */ ADC : origin = 0x007100, length = 0x000080 /* ADC registers */ I2CA : origin = 0x007900, length = 0x000040 /* I2C-A registers */ PARTID : origin = 0x3D7E80, length = 0x000001 /* Part ID register location */ CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations. */ } SECTIONS { /*** PIE Vect Table and Boot ROM Variables Structures ***/ UNION run = PIE_VECT, PAGE = 1 { PieVectTableFile GROUP { EmuKeyVar EmuBModeVar FlashCallbackVar FlashScalingVar } } /*** Peripheral Frame 0 Register Structures ***/ DevEmuRegsFile : > DEV_EMU, PAGE = 1 SysPwrCtrlRegsFile: > SYS_PWR_CTL, PAGE = 1 FlashRegsFile : > FLASH_REGS, PAGE = 1 CsmRegsFile : > CSM, PAGE = 1 AdcResultFile : > ADC_RESULT, PAGE = 1 CpuTimer0RegsFile : > CPU_TIMER0, PAGE = 1 CpuTimer1RegsFile : > CPU_TIMER1, PAGE = 1 CpuTimer2RegsFile : > CPU_TIMER2, PAGE = 1 PieCtrlRegsFile : > PIE_CTRL, PAGE = 1 Cla1RegsFile : > CLA1, PAGE = 1 /*** Peripheral Frame 1 Register Structures ***/ ECanaRegsFile : > ECANA, PAGE = 1 ECanaLAMRegsFile : > ECANA_LAM, PAGE = 1 ECanaMboxesFile : > ECANA_MBOX, PAGE = 1 ECanaMOTSRegsFile : > ECANA_MOTS, PAGE = 1 ECanaMOTORegsFile : > ECANA_MOTO, PAGE = 1 ECap1RegsFile : > ECAP1, PAGE = 1 HRCap1RegsFile : > HRCAP1, PAGE = 1 HRCap2RegsFile : > HRCAP2, PAGE = 1 EQep1RegsFile : > EQEP1, PAGE = 1 LinaRegsFile : > LINA, PAGE = 1 GpioCtrlRegsFile : > GPIOCTRL, PAGE = 1 GpioDataRegsFile : > GPIODAT, PAGE = 1 GpioIntRegsFile : > GPIOINT, PAGE = 1 /*** Peripheral Frame 2 Register Structures ***/ SysCtrlRegsFile : > SYSTEM, PAGE = 1 SpiaRegsFile : > SPIA, PAGE = 1 SpibRegsFile : > SPIB, PAGE = 1 SciaRegsFile : > SCIA, PAGE = 1 NmiIntruptRegsFile: > NMIINTRUPT, PAGE = 1 XIntruptRegsFile : > XINTRUPT, PAGE = 1 AdcRegsFile : > ADC, PAGE = 1 I2caRegsFile : > I2CA, PAGE = 1 /*** Peripheral Frame 3 Register Structures ***/ Comp1RegsFile : > COMP1, PAGE = 1 Comp2RegsFile : > COMP2, PAGE = 1 Comp3RegsFile : > COMP3, PAGE = 1 EPwm1RegsFile : > EPWM1, PAGE = 1 EPwm2RegsFile : > EPWM2, PAGE = 1 EPwm3RegsFile : > EPWM3, PAGE = 1 EPwm4RegsFile : > EPWM4, PAGE = 1 EPwm5RegsFile : > EPWM5, PAGE = 1 EPwm6RegsFile : > EPWM6, PAGE = 1 EPwm7RegsFile : > EPWM7, PAGE = 1 /*** Code Security Module Register Structures ***/ CsmPwlFile : > CSM_PWL, PAGE = 1 /*** Device Part ID Register Structures ***/ PartIdRegsFile : > PARTID, PAGE = 1 }
请大家帮我看一下,谢谢!
哪个memory map怎么看啊,那里面的M0,M1,L0,L1这种和CMD文件的里是一一对应的吗?
memory map对应的是芯片的实际存储空间,CMD文件中各个存储区域的定义不能随便写,
RAML0L1 : origin = 0x000800, length = 0x2F3F00
RAML2 : origin = 0x2F4700, length = 0x100450
你定义的这两个区域明显超出了实际存储区域的地址范围。
RAML3 : origin = 0x3F4B50, length = 0x001000
这一块的地址范围已经是位于Flash区域了。
就是这个图表,例程里边的CMD文件就是跟这个memory map一致。你的text段太大,只能放到Flash中,而且需要合并三个Flash section才能放得下。