TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

错误提示 #10264 PARTID memory range

因为内存不够就把 28033_RAM_lnk.cmd修改了一下,结果DSP2803x_Headers_nonBIOS.cmd就报了这个错误:#10264 PARTID memory range。

28033_RAM_lnk.cmd文件如下。我主要是把RAML0L1改大了。

MEMORY
{
PAGE 0 :
   /* BEGIN is used for the "boot to SARAM" bootloader mode   */

   BEGIN     		: origin = 0x000000, length = 0x000002
   RAMM0      	: origin = 0x000050, length = 0x0003B0
   RAML0L1    	: origin = 0x000800, length = 0x2F3F00
   RESET        	: origin = 0x3FFFC0, length = 0x000002
   IQTABLES   	: origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2  	: origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3 	: origin = 0x3FEBDC, length = 0x0000AA	 /* IQ Math Tables in Boot ROM */

   BOOTROM    : origin = 0x3FF27C, length = 0x000D44


PAGE 1 :

   BOOT_RSVD   : origin = 0x000002, length = 0x00004E     /* Part of M0, BOOT rom will use this for stack */
   RAMM1       : origin = 0x000480, length = 0x000380     /* on-chip RAM block M1 */
   RAML2       : origin = 0x2F4700, length = 0x100450
   RAML3       : origin = 0x3F4B50, length = 0x001000
}


SECTIONS
{
   /* Setup for "boot to SARAM" mode:
      The codestart section (found in DSP28_CodeStartBranch.asm)
      re-directs execution to the start of user code.  */
   codestart        : > BEGIN,     PAGE = 0
   ramfuncs         : > RAMM0      PAGE = 0
   .text            : > RAML0L1,   PAGE = 0
   .cinit           : > RAMM0,     PAGE = 0
   .pinit           : > RAMM0,     PAGE = 0
   .switch          : > RAMM0,     PAGE = 0
   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   .stack           : > RAMM1,     PAGE = 1
   .ebss            : > RAML2,     PAGE = 1
   .econst          : > RAML2,     PAGE = 1
   .esysmem         : > RAML2,     PAGE = 1

   IQmath           : > RAML0L1,   PAGE = 0
   IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD
}

DSP2803x_Headers_nonBIOS.cmd我没有过。

MEMORY
{
 PAGE 0:    /* Program Memory */

 PAGE 1:    /* Data Memory */

   DEV_EMU     : origin = 0x000880, length = 0x000105     /* device emulation registers */
	 SYS_PWR_CTL : origin = 0x000985, length = 0x000003     /* System power control registers */
   FLASH_REGS  : origin = 0x000A80, length = 0x000060     /* FLASH registers */
   CSM         : origin = 0x000AE0, length = 0x000010     /* code security module registers */

   ADC_RESULT  : origin = 0x000B00, length = 0x000020     /* ADC Results register mirror */

   CPU_TIMER0  : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */
   CPU_TIMER1  : origin = 0x000C08, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/
   CPU_TIMER2  : origin = 0x000C10, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/

   PIE_CTRL    : origin = 0x000CE0, length = 0x000020     /* PIE control registers */
   PIE_VECT    : origin = 0x000D00, length = 0x000100     /* PIE Vector Table */

   CLA1        : origin = 0x001400, length = 0x000080     /* CLA registers */

   ECANA       : origin = 0x006000, length = 0x000040     /* eCAN-A control and status registers */
   ECANA_LAM   : origin = 0x006040, length = 0x000040     /* eCAN-A local acceptance masks */
   ECANA_MOTS  : origin = 0x006080, length = 0x000040     /* eCAN-A message object time stamps */
   ECANA_MOTO  : origin = 0x0060C0, length = 0x000040     /* eCAN-A object time-out registers */
   ECANA_MBOX  : origin = 0x006100, length = 0x000100     /* eCAN-A mailboxes */

   COMP1       : origin = 0x006400, length = 0x000020     /* Comparator + DAC 1 registers */
   COMP2       : origin = 0x006420, length = 0x000020     /* Comparator + DAC 2 registers */
   COMP3       : origin = 0x006440, length = 0x000020     /* Comparator + DAC 3 registers */

   EPWM1       : origin = 0x006800, length = 0x000040     /* Enhanced PWM 1 registers */
   EPWM2       : origin = 0x006840, length = 0x000040     /* Enhanced PWM 2 registers */
   EPWM3       : origin = 0x006880, length = 0x000040     /* Enhanced PWM 3 registers */
   EPWM4       : origin = 0x0068C0, length = 0x000040     /* Enhanced PWM 4 registers */
   EPWM5       : origin = 0x006900, length = 0x000040     /* Enhanced PWM 5 registers */
   EPWM6       : origin = 0x006940, length = 0x000040     /* Enhanced PWM 6 registers */
   EPWM7       : origin = 0x006980, length = 0x000040     /* Enhanced PWM 7 registers */

   ECAP1       : origin = 0x006A00, length = 0x000020     /* Enhanced Capture 1 registers */

   HRCAP1      : origin = 0x006AC0, length = 0x000020     /* High Resolution Capture 1 registers */
   HRCAP2      : origin = 0x006AE0, length = 0x000020     /* High Resolution Capture 2 registers */

   EQEP1       : origin = 0x006B00, length = 0x000040     /* Enhanced QEP 1 registers */

   LINA        : origin = 0x006C00, length = 0x000080     /* LIN-A registers */

   GPIOCTRL    : origin = 0x006F80, length = 0x000040     /* GPIO control registers */
   GPIODAT     : origin = 0x006FC0, length = 0x000020     /* GPIO data registers */
   GPIOINT     : origin = 0x006FE0, length = 0x000020     /* GPIO interrupt/LPM registers */

   SYSTEM      : origin = 0x007010, length = 0x000020     /* System control registers */

   SPIA        : origin = 0x007040, length = 0x000010     /* SPI-A registers */
   SPIB        : origin = 0x007740, length = 0x000010     /* SPI-B registers */

   SCIA        : origin = 0x007050, length = 0x000010     /* SCI-A registers */

   NMIINTRUPT  : origin = 0x007060, length = 0x000010     /* NMI Watchdog Interrupt Registers */
   XINTRUPT    : origin = 0x007070, length = 0x000010     /* external interrupt registers */

   ADC         : origin = 0x007100, length = 0x000080     /* ADC registers */

   I2CA        : origin = 0x007900, length = 0x000040     /* I2C-A registers */

   PARTID      : origin = 0x3D7E80, length = 0x000001     /* Part ID register location */

   CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations. */

}


SECTIONS
{
/*** PIE Vect Table and Boot ROM Variables Structures ***/
  UNION run = PIE_VECT, PAGE = 1
   {
      PieVectTableFile
      GROUP
      {
         EmuKeyVar
         EmuBModeVar
         FlashCallbackVar
         FlashScalingVar
      }
   }

/*** Peripheral Frame 0 Register Structures ***/
   DevEmuRegsFile    : > DEV_EMU,     PAGE = 1
	 SysPwrCtrlRegsFile: > SYS_PWR_CTL, PAGE = 1
   FlashRegsFile     : > FLASH_REGS,  PAGE = 1
   CsmRegsFile       : > CSM,         PAGE = 1
   AdcResultFile     : > ADC_RESULT,  PAGE = 1
   CpuTimer0RegsFile : > CPU_TIMER0,  PAGE = 1
   CpuTimer1RegsFile : > CPU_TIMER1,  PAGE = 1
   CpuTimer2RegsFile : > CPU_TIMER2,  PAGE = 1
   PieCtrlRegsFile   : > PIE_CTRL,    PAGE = 1
   Cla1RegsFile      : > CLA1,        PAGE = 1

/*** Peripheral Frame 1 Register Structures ***/
   ECanaRegsFile     : > ECANA,       PAGE = 1
   ECanaLAMRegsFile  : > ECANA_LAM,   PAGE = 1
   ECanaMboxesFile   : > ECANA_MBOX,  PAGE = 1
   ECanaMOTSRegsFile : > ECANA_MOTS,  PAGE = 1
   ECanaMOTORegsFile : > ECANA_MOTO,  PAGE = 1
   ECap1RegsFile     : > ECAP1,       PAGE = 1
   HRCap1RegsFile    : > HRCAP1,      PAGE = 1
   HRCap2RegsFile    : > HRCAP2,      PAGE = 1
   EQep1RegsFile     : > EQEP1,       PAGE = 1
   LinaRegsFile	     : > LINA,        PAGE = 1
   GpioCtrlRegsFile  : > GPIOCTRL,    PAGE = 1
   GpioDataRegsFile  : > GPIODAT,     PAGE = 1
   GpioIntRegsFile   : > GPIOINT,     PAGE = 1

/*** Peripheral Frame 2 Register Structures ***/
   SysCtrlRegsFile   : > SYSTEM,      PAGE = 1
   SpiaRegsFile      : > SPIA,        PAGE = 1
   SpibRegsFile      : > SPIB,        PAGE = 1
   SciaRegsFile      : > SCIA,        PAGE = 1
   NmiIntruptRegsFile: > NMIINTRUPT,  PAGE = 1
   XIntruptRegsFile  : > XINTRUPT,    PAGE = 1
   AdcRegsFile       : > ADC,         PAGE = 1
   I2caRegsFile      : > I2CA,        PAGE = 1

/*** Peripheral Frame 3 Register Structures ***/
   Comp1RegsFile     : > COMP1,    PAGE = 1
   Comp2RegsFile     : > COMP2,    PAGE = 1
   Comp3RegsFile     : > COMP3,    PAGE = 1
   EPwm1RegsFile     : > EPWM1,    PAGE = 1
   EPwm2RegsFile     : > EPWM2,    PAGE = 1
   EPwm3RegsFile     : > EPWM3,    PAGE = 1
   EPwm4RegsFile     : > EPWM4,    PAGE = 1
   EPwm5RegsFile     : > EPWM5,    PAGE = 1
   EPwm6RegsFile     : > EPWM6,    PAGE = 1
   EPwm7RegsFile     : > EPWM7,    PAGE = 1

/*** Code Security Module Register Structures ***/
   CsmPwlFile        : > CSM_PWL,  PAGE = 1

/*** Device Part ID Register Structures ***/
   PartIdRegsFile    : > PARTID,   PAGE = 1

}

请大家帮我看一下,谢谢!

  • RAML0L1    : origin = 0x000800, length = 0x2F3F00

    RAML2       : origin = 0x2F4700, length = 0x100450
       RAML3       : origin = 0x3F4B50, length = 0x001000

    这几个区域的起始地址和长度都是错误的,请根据datasheet中F28033的memory map来修改CMD文件。

     

  • 看了一下你改大后的地址应该也没有超过范围,你将地址改成你修改前仍然报同样的错误吗?

  • 哪个memory map怎么看啊,那里面的M0,M1,L0,L1这种和CMD文件的里是一一对应的吗?

  • Joey Mao,

    没有,报的是28033_RAM_lnk.cmd里的错误,应是说内存不够吧。我截图了:

  • memory map对应的是芯片的实际存储空间,CMD文件中各个存储区域的定义不能随便写,
    RAML0L1    : origin = 0x000800, length = 0x2F3F00
    RAML2       : origin = 0x2F4700, length = 0x100450
    你定义的这两个区域明显超出了实际存储区域的地址范围。

    RAML3       : origin = 0x3F4B50, length = 0x001000
    这一块的地址范围已经是位于Flash区域了。

  • Hank Zhao,

    谢谢你的细心讲解,本人是新手问题比较多,而且幼稚。。。

    你说的实际存储区域的地址范围是这个吗?

    也就是说我一般不需要改写这些东西了?平时应该把.test段写到flash里面?

  • 就是这个图表,例程里边的CMD文件就是跟这个memory map一致。你的text段太大,只能放到Flash中,而且需要合并三个Flash section才能放得下。