This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: 关于死区时间设置

Part Number: TMS320F28335

您好,在设置EPWM死区模块时,用示波器观察输出EPWM波形,发现如下现象。EPWM1A经过死区模块,但是不翻转,示波器观察的是正常波形。但其他条件不变,EPWM1经过死区模块,经过翻转,即配置DBCTL[POLSEL]模块,用示波器观察输出波形,发现EPWM1已经翻转,但翻转前有个短波,且为高电平,请问这一现象怎么解释。

  • 方便发一下配置代码和波形吗?

  • 好的,EPWM代码如下:死区时间为0,频率为100khz.EPWM1和EPWM2配置一样,波形如链接所示,以EPWM1A的上升沿为触发,EPWM1B和EPWM2B在程序中设置了翻转,可以看到出发前有两个短波,而且EPWM1B比EPWM2B短波时间要长。

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    void Init_epwm1(void)
    {
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up-down
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;·
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;·
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Enable phase loading
    EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW; // TBPRD is loaded from its shadow register
    EPwm1Regs.TBPRD = EPWM_PRD; // Set timer period (100kHz)
    EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
    EPwm1Regs.TBCTR = 0x0000; // Clear counter
    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // TBCTR=0
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // CMPA Shadow mode
    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on CTR = 0
    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; // CMPA Shadow mode
    EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Load on CTR = 0
    EPwm1Regs.CMPA.half.CMPA = 2*D* EPWM_PRD; // Initial duty
    EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down CountClear
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • 抱歉刚才操作不当,波形如上图所示

  • 请描述一下测量的操作步骤

  • 1、示波器设定好触发,触发源为EPWM1A,触发电平如图设定为1.2V,且为上升沿触发。四个探头分为接DSP EPWM1A\1B\2A\2B对应的IO口。2、按下给DSP供电电源开关,接通开关,示波器即出现如上波形,捕捉到了第一个PWM波如图上所示。

  • 能否把触发源设置为1B或者2B再观察一下?

  • 把触发源设置为1B后,波形也是一样的。经过测试,1B和2B都经过翻转,如果配置1B和2B不进入死区翻转,第一个波就没有这个短波这个现象。配置为死区翻转后,才会有短波现象。所以考虑这种现象是死区的一种机制,来确保上下桥臂不会直通。

  • 我需要一些时间来看一下