Part Number: TMS320F28335
您好,在设置EPWM死区模块时,用示波器观察输出EPWM波形,发现如下现象。EPWM1A经过死区模块,但是不翻转,示波器观察的是正常波形。但其他条件不变,EPWM1经过死区模块,经过翻转,即配置DBCTL[POLSEL]模块,用示波器观察输出波形,发现EPWM1已经翻转,但翻转前有个短波,且为高电平,请问这一现象怎么解释。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
您好,在设置EPWM死区模块时,用示波器观察输出EPWM波形,发现如下现象。EPWM1A经过死区模块,但是不翻转,示波器观察的是正常波形。但其他条件不变,EPWM1经过死区模块,经过翻转,即配置DBCTL[POLSEL]模块,用示波器观察输出波形,发现EPWM1已经翻转,但翻转前有个短波,且为高电平,请问这一现象怎么解释。
好的,EPWM代码如下:死区时间为0,频率为100khz.EPWM1和EPWM2配置一样,波形如链接所示,以EPWM1A的上升沿为触发,EPWM1B和EPWM2B在程序中设置了翻转,可以看到出发前有两个短波,而且EPWM1B比EPWM2B短波时间要长。
void Init_epwm1(void)
{
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up-down
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Enable phase loading
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW; // TBPRD is loaded from its shadow register
EPwm1Regs.TBPRD = EPWM_PRD; // Set timer period (100kHz)
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // 同步信号输出选择TBCTR=0
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // CMPA Shadow mode
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on CTR = 0
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; // CMPA Shadow mode
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Load on CTR = 0
EPwm1Regs.CMPA.half.CMPA = 2*D* EPWM_PRD; // Initial duty
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down Count:Clear
EPwm1Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // TBCTR = CMPA on Up Count:NO ACTION
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // TBCTR = 0 on Up Count:Set
EPwm1Regs.AQCTLB.bit.CAU = AQ_NO_ACTION;
EPwm1Regs.AQCTLB.bit.CAD = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //0x3 MODE2 AHC high level delay (AHC)死区双边使能
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //0x2 A不反转,B反转
EPwm1Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
EPwm1Regs.DBRED = EPWM1_DBRED;
EPwm1Regs.DBFED = EPWM1_DBFED;
}
void Init_epwm2(void)
{
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up-down
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Enable phase loading
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW; // TBPRD is loaded from its shadow register
EPwm2Regs.TBPRD = EPWM_PRD;
EPwm2Regs.TBPHS.half.TBPHS = 0;
EPwm2Regs.TBCTR = 0x0000; // Clear counter
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // CMPA Shadow mode
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on CTR = 0
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; // CMPA Shadow mode
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Load on CTR = 0
EPwm2Regs.CMPA.half.CMPA = 2*D* EPWM_PRD; // Initial duty
EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down Count:Clear
EPwm2Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // TBCTR = CMPA on Up Count:NO ACTION
EPwm2Regs.AQCTLA.bit.ZRO = AQ_SET; // TBCTR = 0 on Up Count:Set
EPwm2Regs.AQCTLB.bit.CAU = AQ_NO_ACTION;
EPwm2Regs.AQCTLB.bit.CAD = AQ_CLEAR;
EPwm2Regs.AQCTLB.bit.ZRO = AQ_SET;
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //0x3 MODE2 AHC high level delay (AHC)死区双边使能
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //0x2 A不反转,B反转
EPwm2Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
EPwm2Regs.DBRED = EPWM2_DBRED;
EPwm2Regs.DBFED = EPWM2_DBFED;
}