This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: 28338PWM配置问题

Part Number: TMS320F28335

请问这个问题有什么解释吗?

  • 不好意思之前漏掉了。

    有两点我需要再确认一下:

    1. 初始化ePWM模块的流程是怎样的?也就是说在初始化之前有没有关闭ePWM模块的外设时钟,然后在配置完成后再打开?

    2. 试一下在配置的最后再手动清一下TBCTR。

  • void Init_EPWM()
    {
        EALLOW;
        SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Disable TBCLK within the EPWM
        EDIS;
        
        Init_epwm1();
        Init_epwm2();
        // Init_epwm3();
        
        EALLOW;
        SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Enable TBCLK within the EPWM
        EDIS;
    }
    
    //=======================================================
    //函数名称: Init_epwm1()
    //功能: 初始化EPWM1为带死区互补输出(AHC)的可变频率的PWM 逆变级
    //输入:
    //返回:
    //备注:
    //=======================================================
    void Init_epwm1(void)
    {
    
        EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up-down
        EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = EPWMCLK /(HSPCLKDIV× CLKDIV)
        EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1; // TBCLK = 150M/(1*1)= 150MHz
        EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Enable phase loading
        EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW; // TBPRD is loaded from its shadow register
        
        EPwm1Regs.TBPRD = EPWM_PRD; // Set timer period (100kHz)
        EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
        EPwm1Regs.TBCTR = 0x0000; // Clear counter
        EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // 同步信号输出选择TBCTR=0
        EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // CMPA Shadow mode
        EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on CTR = 0
        EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; // CMPA Shadow mode
        EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Load on CTR = 0
        
        EPwm1Regs.CMPA.half.CMPA = 2*D* EPWM_PRD; // Initial duty
        
        EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down Count:Clear
        EPwm1Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // TBCTR = CMPA on Up Count:NO ACTION
        EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // TBCTR = 0 on Up Count:Set
        
        // EPwm1Regs.AQCTLB.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down Count:Clear
        // EPwm1Regs.AQCTLB.bit.CAD = AQ_NO_ACTION; // TBCTR = CMPA on Up Count:NO ACTION
        // EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET; // T BCTR = 0 on Up Count:Set
        
        EPwm1Regs.AQCTLB.bit.CAU = AQ_NO_ACTION;
        EPwm1Regs.AQCTLB.bit.CAD = AQ_CLEAR;
        EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;
        //DELAY_US(100000);
        EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //0x3 MODE2 AHC high level delay (AHC)死区双边使能
        EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //0x2 A不反转,B反转
        EPwm1Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
        
        EPwm1Regs.DBRED = EPWM1_DBRED; // 上升沿延时 注意:只有10位,最大1023
        EPwm1Regs.DBFED = EPWM1_DBFED; // 下降沿延时 注意:只有10位,最大1023
        
        EALLOW;
        EPwm1Regs.TZSEL.bit.OSHT1 = 1; //单次触发联防
        // EPwm1Regs.TZSEL.bit.OSHT2 = 1; //单次触发联防
        
        EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO; //强制A低电平
        EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO; //强制B低电平
        //
        // // Enable TZ interrupt
        //
        EPwm1Regs.TZEINT.bit.OST = 1;
        EDIS;
        //
        EALLOW;
        EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; //过零点触发中断
        EPwm1Regs.ETSEL.bit.INTEN = 1; //使能中断
        EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; //每次过零产生中断
        EDIS;
        
        
        //计数器计数等于0时触发ADC转换
        // EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_ZERO; // Counter = 0
        // EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST; // Generate SOCA pulse on 1st event
        // EPwm1Regs.ETCLR.bit.SOCA = 1; // Clear SOCA flag
        // EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOCA
        
        // EPwm1Regs.ETCLR.bit.INT = 1; // Clear INT flag
        // EPwm1Regs.ETSEL.bit.INTEN = 0; // Disable INT
    }
    
    
    
    void Init_epwm2(void)
    {
    
    
        EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up-down
        EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = EPWMCLK /(HSPCLKDIV× CLKDIV)
        EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1; // TBCLK = 150M/(1*1)= 150MHz
        EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Enable phase loading
        EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW; // TBPRD is loaded from its shadow register
        
        EPwm2Regs.TBPRD = EPWM_PRD; // Set timer period (4.8kHz)
        
        EPwm2Regs.TBPHS.half.TBPHS = 0;
        EPwm2Regs.TBCTR = 0x0000; // Clear counter
        EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // 同步信号输出选择外部同步信号输入EPWMxSYNCO
        
        EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // CMPA Shadow mode
        EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on CTR = 0
        EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; // CMPA Shadow mode
        EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Load on CTR = 0
        
        
        EPwm2Regs.CMPA.half.CMPA = 2*D* EPWM_PRD; // Initial duty
        
        // EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down Count:Clear
        // EPwm2Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // TBCTR = CMPA on Up Count:NO ACTION
        // EPwm2Regs.AQCTLA.bit.ZRO = AQ_SET; // TBCTR = 0 on Up Count:Set
        //
        // EPwm2Regs.AQCTLB.bit.CAU = AQ_NO_ACTION;
        // EPwm2Regs.AQCTLB.bit.CAD = AQ_CLEAR;
        // EPwm2Regs.AQCTLB.bit.ZRO = AQ_SET;
        //
        // EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //0x3 MODE2 AHC high level delay (AHC)死区双边使能
        // EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //0x1 A不反转,B反转
        // EPwm2Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
        
        // EPwm2Regs.AQCTLA.bit.CAU = AQ_NO_ACTION; // TBCTR = CMPA on Down Count:Clear
        // EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // TBCTR = CMPA on Up Count:Set
        // EPwm2Regs.AQCTLA.bit.ZRO = AQ_CLEAR;
        //
        // EPwm2Regs.AQCTLB.bit.CAU = AQ_SET;
        // EPwm2Regs.AQCTLB.bit.CAD = AQ_NO_ACTION;
        // EPwm2Regs.AQCTLB.bit.ZRO = AQ_CLEAR;
        EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down Count:Clear
        EPwm2Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // TBCTR = CMPA on Up Count:NO ACTION
        EPwm2Regs.AQCTLA.bit.ZRO = AQ_SET; // TBCTR = 0 on Up Count:Set
        
        // EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // TBCTR = CMPA on Down Count:Clear
        // EPwm2Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // TBCTR = CMPA on Up Count:NO ACTION
        // EPwm2Regs.AQCTLA.bit.ZRO = AQ_NO_ACTION; // TBCTR = 0 on Up Count:Set
        //
        // EPwm2Regs.AQCTLB.bit.CAU = AQ_CLEAR;
        // EPwm2Regs.AQCTLB.bit.CAD = AQ_NO_ACTION;
        // EPwm2Regs.AQCTLB.bit.ZRO = AQ_NO_ACTION;
        
        EPwm2Regs.AQCTLB.bit.CAU = AQ_NO_ACTION;
        EPwm2Regs.AQCTLB.bit.CAD = AQ_CLEAR;
        EPwm2Regs.AQCTLB.bit.ZRO = AQ_SET;
        
        EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //0x3 MODE2 AHC high level delay (AHC)死区双边使能
        EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //0x2 A不反转,B反转
        // EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HI; //0x2 A不反转,B不反转
        EPwm2Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
        
        // EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //0x3 MODE2 AHC high level delay (AHC)死区双边使能
        // EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //0x2
        // EPwm2Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
        
        EPwm2Regs.DBRED = EPWM2_DBRED; // 上升沿延时 上升死区为0.5%的占空比 0.5%个TBPRD(150MHz) 注意:只有10位,最大1023
        EPwm2Regs.DBFED = EPWM2_DBFED; // 下降沿延时 下降死区为0.5%的占空比 0.5%个TBPRD(150MHz) 注意:只有10位,最大1023
        
        
        
        EALLOW;
        
        EPwm2Regs.TZSEL.bit.OSHT1 = 1;
        EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO;
        EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO;
        
        
        //Enable TZ interrupt
        
        // EPwm2Regs.TZEINT.bit.CBC =1;
        EPwm2Regs.TZEINT.bit.OST = 1;
        EDIS;
        
        // EALLOW;
        // //EPwm1Regs.AQCSFRC.all=0x05; //强制低
        // EPwm2Regs.AQCSFRC.all=0x05; //强制低
        // // EPwm3Regs.AQCSFRC.all=0x05;
        // // EPwm6Regs.AQCSFRC.all=0x05;
        // EPwm2Regs.DBCTL.bit.POLSEL = 0x0; //不反转极性
        // EDIS;
    }

    如图上代码所示,Init_EPWM()为PWM初始化函数,其流程是先关闭TBCLKSYNC时基时钟,再进行配置,配置结束后再开启时基时钟。另外你说的外设时钟,不知道是不是这片代码。这片代码在工程文件的DSP2833x_SysCtrl.c源文件里,并未改动。

    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Disable TBCLK within the ePWM
    SysCtrlRegs.PCLKCR1.bit.EPWM1ENCLK = 1; // ePWM1
    SysCtrlRegs.PCLKCR1.bit.EPWM2ENCLK = 1; // ePWM2
    SysCtrlRegs.PCLKCR1.bit.EPWM3ENCLK = 1; // ePWM3
    SysCtrlRegs.PCLKCR1.bit.EPWM4ENCLK = 1; // ePWM4
    SysCtrlRegs.PCLKCR1.bit.EPWM5ENCLK = 1; // ePWM5
    SysCtrlRegs.PCLKCR1.bit.EPWM6ENCLK = 1; // ePWM6
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Enable TBCLK within the ePWM
     

    2.配置完后清除了TBCLR计数器,还是有这个现象。

    3,这个现象出现在在翻转的那一路PWM上,不论PWM动作模块怎么配置,只要在死区模块中把该路PWM翻转,PWM输出不论输出高电平,还是低电平,第一个脉冲时钟就有一段高电平。这段高电平过后就是正常的PWM波。这个现象也出现在直接购买的28335开发板上。

  • 我复现到了你描述的现象

  • 为了方便之后查看,我把DB的配置发上来:

    另外为了方便查看,我把你之前上传的代码的格式改了一下

  • 对,是这种配置,这个现象会导致我们电路会发生保护。而且EPWM1B这段高电平持续时间高一些,EPWM2B高电平持续时间低一些。

  • 关键配置:

    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    
    EPwm1Regs.TBCTR = 0x0000;
    
    EPwm1Regs.CMPA.half.CMPA = 2 * D * EPWM_PRD;
    
    EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET;
    
    EPwm1Regs.AQCTLB.bit.CAD = AQ_CLEAR;
    EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;
    
    EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
    EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;       //B reverse
    EPwm1Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
    
    EPwm1Regs.DBRED = EPWM1_DBRED;
    EPwm1Regs.DBFED = EPWM1_DBFED;

    实验结果:

    第1、第2个波形分别是第一个PWM波之前的高电平脉冲以及它的宽度;

    第3个波形是之后的PWM波。

    黄色的是1A,紫色的是1B。

    不难看出,1B脉冲的下降沿 到 1A的上升沿 之间是设定的1A的上升沿延迟。

    根据实验推断的原因是DB模块中存在延时。

    1B的配置是0处置1,CAD处清0;但是加入了翻转,也就是说实际上是在CAD附近置1,紧接着在0处清0。

    上面提到的DB模块中的延时为低电平,是在第一个0处清零(翻转前是置高)之前,被翻转了上去,所以产生了脉冲。

  • 谢谢回答,您的意思是PWM信号在经过死区模块中翻转的那一部分,即DBCTL(POLSEL)这个部分存在延迟吗?这个延迟时间也不是固定的,那这个问题是固有的,没办法消除这段高电平是吗,

  • 目前不确定具体是DB中的哪一部分存在延迟;数据手册中确实也没有提到。有可能存在于极性翻转这里;也有可能不是,因为翻转之后才会在波形中体现出来。

    这个我需要再实验以及与其他工程师讨论一下。

    目前最快的解决办法就是先不要用极性翻转,通过不同的动作来实现A路与B路之间的互补。