Other Parts Discussed in Thread: C2000WARE
专家你好,我使用CCS配置CLA,生成后套用C盘软件安装目录里C2000Ware_5_00_00_00里的cla_ex1_asin模板。asin
使用模板能够正常调试CLA,也能在CLA里单步调试,能正常使用。
但是将模板的主要代码asin.cla、cla_ex1_asin_shared.h,还有其他代码移植到我的工程后无法正常调试和使用CLA。
具体现象如下:1.Cla1ProgRunStart能够将CLA程序从Flash拷贝到RAMLS0,memory中有显示相关代码。
2.在DEBUG界面CLA,Load Symbols后显示no symbols are defined
3.运行CLA_runTest()时y数组没有变化,y数值依然是初始值0。
board.c部分相关代码如下:
#include "board.h"
//*****************************************************************************
//
// Board Configurations
// Initializes the rest of the modules.
// Call this function in your application if you wish to do all module
// initialization.
// If you wish to not use some of the initializations, instead of the
// Board_init use the individual Module_inits
//
//*****************************************************************************
void Board_init()
{
EALLOW;
PinMux_init();
SYNC_init();
ASYSCTL_init();
CLA_init();
MEMCFG_init();
ADC_init();
AIO_init();
CPUTIMER_init();
EPWM_init();
GPIO_init();
PGA_init();
INTERRUPT_init();
EDIS;
}
//*****************************************************************************
//
// CLA Configurations
//
//*****************************************************************************
void myCLA0_init(){
//
// Configure all CLA task vectors
// On Type-1 and Type-2 CLAs the MVECT registers accept full 16-bit task addresses as
// opposed to offsets used on older Type-0 CLAs
//
#pragma diag_suppress=770
//
// CLA Task 1
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_1, (uint16_t)&Cla1Task1);
CLA_setTriggerSource(CLA_TASK_1, CLA_TRIGGER_SOFTWARE);
//
// CLA Task 2
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_2, (uint16_t)&Cla1Task2);
CLA_setTriggerSource(CLA_TASK_2, CLA_TRIGGER_SOFTWARE);
//
// CLA Task 3
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_3, (uint16_t)&Cla1Task3);
CLA_setTriggerSource(CLA_TASK_3, CLA_TRIGGER_SOFTWARE);
//
// CLA Task 4
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_4, (uint16_t)&Cla1Task4);
CLA_setTriggerSource(CLA_TASK_4, CLA_TRIGGER_SOFTWARE);
//
// CLA Task 5
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_5, (uint16_t)&Cla1Task5);
CLA_setTriggerSource(CLA_TASK_5, CLA_TRIGGER_SOFTWARE);
//
// CLA Task 6
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_6, (uint16_t)&Cla1Task6);
CLA_setTriggerSource(CLA_TASK_6, CLA_TRIGGER_SOFTWARE);
//
// CLA Task 7
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_7, (uint16_t)&Cla1Task7);
CLA_setTriggerSource(CLA_TASK_7, CLA_TRIGGER_SOFTWARE);
//
// CLA Task 8
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_8, (uint16_t)&Cla1Task8);
CLA_setTriggerSource(CLA_TASK_8, CLA_TRIGGER_SOFTWARE);
//
// Disable background task
//
CLA_disableBackgroundTask(myCLA0_BASE);
#pragma diag_warning=770
//
// Enable the IACK instruction to start a task on CLA in software
// for all 8 CLA tasks. Also, globally enable all 8 tasks (or a
// subset of tasks) by writing to their respective bits in the
// MIER register
//
CLA_enableIACK(myCLA0_BASE);
CLA_enableTasks(myCLA0_BASE, CLA_TASKFLAG_ALL);
}
void CLA_init()
{
#ifdef _FLASH
#ifndef CMDTOOL // Linker command tool is not used
extern uint32_t Cla1ProgRunStart, Cla1ProgLoadStart, Cla1ProgLoadSize;
extern uint32_t Cla1ConstRunStart, Cla1ConstLoadStart, Cla1ConstLoadSize;
//
// Copy the program and constants from FLASH to RAM before configuring
// the CLA
//
memcpy((uint32_t *)&Cla1ProgRunStart, (uint32_t *)&Cla1ProgLoadStart,
(uint32_t)&Cla1ProgLoadSize);
memcpy((uint32_t *)&Cla1ConstRunStart, (uint32_t *)&Cla1ConstLoadStart,
(uint32_t)&Cla1ConstLoadSize );
#endif //CMDTOOL
#endif //_FLASH
myCLA0_init();
}
//*****************************************************************************
//
// INTERRUPT Configurations
//
//*****************************************************************************
void INTERRUPT_init(){
// Interrupt Setings for INT_myCLA01
Interrupt_register(INT_myCLA01, &cla1Isr1);
Interrupt_enable(INT_myCLA01);
// Interrupt Setings for INT_myCLA02
Interrupt_register(INT_myCLA02, &cla1Isr2);
Interrupt_enable(INT_myCLA02);
// Interrupt Setings for INT_myCLA03
Interrupt_register(INT_myCLA03, &cla1Isr3);
Interrupt_enable(INT_myCLA03);
// Interrupt Setings for INT_myCLA04
Interrupt_register(INT_myCLA04, &cla1Isr4);
Interrupt_enable(INT_myCLA04);
// Interrupt Setings for INT_myCLA05
Interrupt_register(INT_myCLA05, &cla1Isr5);
Interrupt_enable(INT_myCLA05);
// Interrupt Setings for INT_myCLA06
Interrupt_register(INT_myCLA06, &cla1Isr6);
Interrupt_enable(INT_myCLA06);
// Interrupt Setings for INT_myCLA07
Interrupt_register(INT_myCLA07, &cla1Isr7);
Interrupt_enable(INT_myCLA07);
// Interrupt Setings for INT_myCLA08
Interrupt_register(INT_myCLA08, &cla1Isr8);
Interrupt_enable(INT_myCLA08);
// Interrupt Setings for INT_timer2
Interrupt_register(INT_timer2, &portTICK_ISR);
Interrupt_disable(INT_timer2);
// Interrupt Setings for INT_myADCA_1
Interrupt_register(INT_myADCA_1, &adcA1ISR);
Interrupt_enable(INT_myADCA_1);
// Interrupt Setings for INT_myADCB_1
Interrupt_register(INT_myADCB_1, &INT_myADCB_1_ISR);
Interrupt_enable(INT_myADCB_1);
// Interrupt Setings for INT_myADCB_4
Interrupt_register(INT_myADCB_4, &INT_myADCB_4_ISR);
Interrupt_enable(INT_myADCB_4);
// Interrupt Setings for INT_myADCC_1
Interrupt_register(INT_myADCC_1, &INT_myADCC_1_ISR);
Interrupt_enable(INT_myADCC_1);
// Interrupt Setings for INT_myADCC_2
Interrupt_register(INT_myADCC_2, &INT_myADCC_2_ISR);
Interrupt_enable(INT_myADCC_2);
// Interrupt Setings for INT_myADCC_3
Interrupt_register(INT_myADCC_3, &INT_myADCC_3_ISR);
Interrupt_enable(INT_myADCC_3);
// Interrupt Setings for INT_myADCC_4
Interrupt_register(INT_myADCC_4, &INT_myADCC_4_ISR);
Interrupt_enable(INT_myADCC_4);
}
main.c代码如下:
//#############################################################################
//
//
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "board.h"
#include "device.h"
#include "clocktree.h"
#define MSGCOUNT 10000
const char gcs8_Software_Version[19] = {'V','A','S','8','6','2','S','0','0','1',0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF};//VAS341C110;
const char gcs8_Hardware_Version[14] = {'V','A','1','0','5','1','-','0','0','1','T'};//VA1064A-002A;
const char gcs8_PCB_Version[12] = {'V','A','1','0','5','1','-','0','0','1','T'};//VA1060A-003A;
#include "cla_ex1_asin_shared.h"
//
// Defines
//
#define WAITSTEP asm(" RPT #255 || NOP")
//
// Globals
//
//
//Task 1 (C) Variables
// NOTE: Do not initialize the Message RAM variables globally, they will be
// reset during the message ram initialization phase in the CLA memory
// configuration routine
//
#ifdef __cplusplus
#pragma DATA_SECTION("CpuToCla1MsgRAM");
float fVal;
#pragma DATA_SECTION("Cla1ToCpuMsgRAM");
float fResult;
#else
#pragma DATA_SECTION(fVal,"CpuToCla1MsgRAM");
float fVal;
#pragma DATA_SECTION(fResult,"Cla1ToCpuMsgRAM");
float fResult;
#endif //__cplusplus
float y[BUFFER_SIZE];
//
//Task 2 (C) Variables
//
//
//Task 3 (C) Variables
//
//
//Task 4 (C) Variables
//
//
//Task 5 (C) Variables
//
//
//Task 6 (C) Variables
//
//
//Task 7 (C) Variables
//
//
//Task 8 (C) Variables
//
//
//Common (C) Variables
//The Exponential table
//
#ifdef __cplusplus
#pragma DATA_SECTION("CLADataLS1")
#else
#pragma DATA_SECTION(CLAasinTable,"CLADataLS1")
#endif //__cplusplus
float CLAasinTable[]={
0.0, 1.0, 0.0,
0.000000636202, 0.999877862610, 0.007815361896,
0.000005099694, 0.999510644409, 0.015647916155,
0.000017268312, 0.998895919094, 0.023514960332,
0.000041121765, 0.998029615282, 0.031434003631,
0.000080794520, 0.996905974725, 0.039422875916,
0.000140631089, 0.995517492804, 0.047499840611,
0.000225244584, 0.993854840311, 0.055683712914,
0.000339579512, 0.991906765146, 0.063993984848,
0.000488979852, 0.989659972212, 0.072450958820,
0.000679263611, 0.987098979366, 0.081075891529,
0.000916805182, 0.984205946802, 0.089891150305,
0.001208627040, 0.980960476685, 0.098920384204,
0.001562502549, 0.977339379243, 0.108188712551,
0.001987071928, 0.973316400729, 0.117722933997,
0.002491973784, 0.968861907789, 0.127551759665,
0.003087995053, 0.963942521723, 0.137706074532,
0.003787242692, 0.958520694794, 0.148219231941,
0.004603341138, 0.952554219267, 0.159127386977,
0.005551660294, 0.945995657913, 0.170469875522,
0.006649579796, 0.938791682505, 0.182289647088,
0.007916796475, 0.930882303984, 0.194633761132,
0.009375683410, 0.922199974574, 0.207553958472,
0.011051710808, 0.912668537890, 0.221107321885,
0.012973941175, 0.902201997769, 0.235357042896,
0.015175614174, 0.890703070035, 0.250373315541,
0.017694840102, 0.878061473098, 0.266234382514,
0.020575425537, 0.864151902887, 0.283027765009,
0.023867860513, 0.848831624374, 0.300851714968,
0.027630504055, 0.831937595031, 0.319816937941,
0.031931014547, 0.813283013821, 0.340048646894,
0.036848083955, 0.792653161200, 0.361689022958,
0.042473551274, 0.769800358920, 0.384900179460,
0.048914992206, 0.744437830278, 0.409867752228,
0.056298910750, 0.716232177740, 0.436805274317,
0.064774696786, 0.684794109766, 0.465959540059,
0.074519565699, 0.649666934178, 0.497617226179,
0.085744766889, 0.610312179660, 0.532113122767,
0.098703445606, 0.566091493186, 0.569840443472,
0.113700678529, 0.516243664372, 0.611263845480,
0.131106395009, 0.459855210927, 0.656936015611,
0.151372169232, 0.395822366759, 0.707518998893,
0.175053263659, 0.322801460177, 0.763811905770,
0.202837883870, 0.239143420888, 0.826787304376,
0.235586468765, 0.142806299514, 0.897639596948,
0.274385149825, 0.031236880585, 0.977850174820,
0.320619535938, -0.098791845166, 1.069276441800,
0.376078169620, -0.251407364538, 1.174275392129,
0.443100143614, -0.431959397725, 1.295878193174,
0.524789871827, -0.647485610469, 1.438041695773,
0.625336471263, -0.907400624736, 1.606018804842,
0.750500589935, -1.224540947101, 1.806917563896,
0.908377657341, -1.616794995066, 2.050569262035,
1.110633894185, -2.109729648039, 2.350920816737,
1.374584721437, -2.740985157716, 2.728353889708,
1.726848242753, -3.567962877198, 3.213722960014,
2.210117561056, -4.682006534082, 3.855770086891,
2.896554011854, -6.236312386687, 4.735651038017,
3.916505715382, -8.505488022524, 5.997790945975,
5.526855868703, -12.026617159136, 7.922628470498,
8.298197116322, -17.983705080358, 11.123941286820,
13.741706072449, -29.488929624542, 17.203344479111,
27.202707817485, -57.466598393615, 31.741016484669,
83.158101335898, -171.803399517566, 90.149831709374
};
float asin_expected[BUFFER_SIZE]={
1.570796, 1.393789, 1.320141, 1.263401, 1.215375,
1.172892, 1.134327, 1.098718, 1.065436, 1.034046,
1.004232, 0.9757544, 0.9484279, 0.9221048, 0.8966658,
0.8720123, 0.8480621, 0.8247454, 0.8020028, 0.7797828,
0.7580408, 0.7367374, 0.7158381, 0.6953120, 0.6751316,
0.6552721, 0.6357113, 0.6164289, 0.5974064, 0.5786270,
0.5600753, 0.5417370, 0.5235988, 0.5056486, 0.4878751,
0.4702678, 0.4528166, 0.4355124, 0.4183464, 0.4013104,
0.3843968, 0.3675981, 0.3509074, 0.3343180, 0.3178237,
0.3014185, 0.2850964, 0.2688521, 0.2526802, 0.2365756,
0.2205333, 0.2045484, 0.1886164, 0.1727327, 0.1568929,
0.1410927, 0.1253278, 0.1095943, 0.09388787, 0.07820469,
0.06254076, 0.04689218, 0.03125509, 0.01562564
};
uint16_t pass = 0;
uint16_t fail = 0;
//
// Function Prototypes
//
void CLA_runTest(void);
__interrupt void cla1Isr1();
__interrupt void cla1Isr2();
__interrupt void cla1Isr3();
__interrupt void cla1Isr4();
__interrupt void cla1Isr5();
__interrupt void cla1Isr6();
__interrupt void cla1Isr7();
__interrupt void cla1Isr8();
void main(void)
{
demo_mea();
Device_init();
Device_initGPIO();
Interrupt_initModule();
Interrupt_initVectorTable();
Can_Drv_Init();
Can_SetConfig();
Hardware_initialization_and_enable();
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
// Can_Test();
// Ccp_Init();
// EcuM_Init();
//
// Run the test
//
CLA_runTest();
for(;;)
{
}
// while(1)
// {
//
// }
//
// Stop application after completion.
//
asm(" ESTOP0");
}
//
// CLA_runTest - Execute CLA task tests for specified vectors
//
void CLA_runTest(void)
{
int16_t i;
float error;
for(i = 0; i < BUFFER_SIZE; i++)
{
fVal= (float)(BUFFER_SIZE - i)/(float)BUFFER_SIZE;
CLA_forceTasks(myCLA0_BASE,CLA_TASKFLAG_1);
WAITSTEP;
y[i] = fResult;
error = fabsf(asin_expected[i]-y[i]);
if(error < 0.1f)
{
pass++;
}
else
{
fail++;
}
}
#if 0
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_2);
WAITSTEP;
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_3);
WAITSTEP;
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_4);
WAITSTEP;
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_5);
WAITSTEP;
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_6);
WAITSTEP;
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_7);
WAITSTEP;
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_8);
WAITSTEP;
#endif
}
//
// cla1Isr1 - CLA1 ISR 1
//
__interrupt void cla1Isr1 ()
{
//
// Acknowledge the end-of-task interrupt for task 1
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP11);
//
// Uncomment to halt debugger and stop here
//
// asm(" ESTOP0");
}
//
// cla1Isr2 - CLA1 ISR 2
//
__interrupt void cla1Isr2 ()
{
asm(" ESTOP0");
}
//
// cla1Isr3 - CLA1 ISR 3
//
__interrupt void cla1Isr3 ()
{
asm(" ESTOP0");
}
//
// cla1Isr4 - CLA1 ISR 4
//
__interrupt void cla1Isr4 ()
{
asm(" ESTOP0");
}
//
// cla1Isr5 - CLA1 ISR 5
//
__interrupt void cla1Isr5 ()
{
asm(" ESTOP0");
}
//
// cla1Isr6 - CLA1 ISR 6
//
__interrupt void cla1Isr6 ()
{
asm(" ESTOP0");
}
//
// cla1Isr7 - CLA1 ISR 7
//
__interrupt void cla1Isr7 ()
{
asm(" ESTOP0");
}
//
// cla1Isr8 - CLA1 ISR 8
//
__interrupt void cla1Isr8 ()
{
//
// Acknowledge the end-of-task interrupt for task 8
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP11);
//
// Uncomment to halt debugger and stop here
//
// asm(" ESTOP0");
}
//
// End of File
//
28004x_generic_flash_lnk.cmd代码如下:
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x0000F6, length = 0x00030A
RAMLS0 : origin = 0x008000, length = 0x001000
RAMLS3 : origin = 0x00A000, length = 0x000800
/* RAMLS4 : origin = 0x00A000, length = 0x000800 */
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
// FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x000100 /* on-chip Flash */
FLASH_BANK0_SEC81 : origin = 0x088100, length =0x000F00 /* on-chip Flash */ //drc
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000 /* on-chip Flash */
/* BANK 1 */
FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0 /* on-chip Flash */
// FLASH_BANK1_SEC15_RSVD : origin = 0x09FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMLS1 : origin = 0x009000, length = 0x000800
RAMLS2 : origin = 0x009800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x001800
/* RAMLS5 : origin = 0x00A800, length = 0x002800//shc-yuanlai
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800 */
RAMGS0 : origin = 0x00C000, length = 0x002000
RAMGS1 : origin = 0x00E000, length = 0x002000
RAMGS2 : origin = 0x010000, length = 0x002000
RAMGS3 : origin = 0x012000, length = 0x001FF8
// RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
codestart : > FLASH_BANK0_SEC8, PAGE = 0, ALIGN(4) /*BEGIN*/
.mcuver1 : > FLASH_BANK0_SEC81, PAGE = 0, ALIGN(4)
.text : >> FLASH_BANK0_SEC10 | FLASH_BANK0_SEC11 | FLASH_BANK0_SEC12 | FLASH_BANK0_SEC13 | FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15 | FLASH_BANK1_SEC0 | FLASH_BANK1_SEC1 , PAGE = 0, ALIGN(4) /*| FLASH_BANK0_SEC8*/
.cinit : > FLASH_BANK0_SEC9, PAGE = 0, ALIGN(4)
.switch : > FLASH_BANK0_SEC9, PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
#if defined(__TI_EABI__)
.init_array : > FLASH_BANK0_SEC9, PAGE = 0, ALIGN(4)
.bss : > RAMLS5, PAGE = 1
.bss:output : > RAMLS3, PAGE = 0
.bss:cio : > RAMLS0, PAGE = 0
.data : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
/* Initalized sections go in Flash */
.const : > FLASH_BANK0_SEC12, PAGE = 0, ALIGN(4)
#else
.pinit : > FLASH_BANK0_SEC9, PAGE = 0, ALIGN(4)
.ebss : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
.cio : > RAMLS0, PAGE = 0
.econst : > FLASH_BANK0_SEC12, PAGE = 0, ALIGN(4)
#endif
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
ramgs2 : > RAMGS2, PAGE = 1
ramgs3 : > RAMGS3, PAGE = 1
#if defined(__TI_EABI__)
/* CLA specific sections */
Cla1Prog : LOAD = FLASH_BANK0_SEC11,
RUN = RAMLS0,
LOAD_START(Cla1ProgLoadStart),
RUN_START(Cla1ProgRunStart),
LOAD_SIZE(Cla1ProgLoadSize),
PAGE = 0, ALIGN(4)
#else
/* CLA specific sections */
Cla1Prog : LOAD = FLASH_BANK0_SEC11,
RUN = RAMLS0,
LOAD_START(_Cla1ProgLoadStart),
RUN_START(_Cla1ProgRunStart),
LOAD_SIZE(_Cla1ProgLoadSize),
PAGE = 0, ALIGN(4)
#endif
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
#if defined(__TI_EABI__)
.TI.ramfunc : LOAD = FLASH_BANK0_SEC9,
RUN = RAMLS0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
.TI.ramfunc : LOAD = FLASH_BANK0_SEC9,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
.scratchpad : > RAMLS1, PAGE = 1
.bss_cla : > RAMLS1, PAGE = 1
Cla1DataRam : > RAMLS2, PAGE = 1
cla_shared : > RAMLS1, PAGE = 1
CLADataLS1 : > RAMLS1, PAGE = 1
#if defined(__TI_EABI__)
.const_cla : LOAD = FLASH_BANK0_SEC10,
RUN = RAMLS3,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
PAGE = 0, ALIGN(4)
#else
.const_cla : LOAD = FLASH_BANK0_SEC10,
RUN = RAMLS3,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
PAGE = 0, ALIGN(4)
#endif
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/