Part Number: TMS320F28377D
Hi, I tried to configure SPIA from CPU02, without success. When I go into debug mode and pause the code, the code gets stuck in the while((HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLSTS) &
SYSCTL_SYSPLLSTS_LOCKS) == 0U) Not quite sure why this is happening. Before this, all of the functions were already tested on CPU01 and ran brilliantly.
Here are some snippets of the code in core1:
Device_init();
Device_initGPIO();
// GPIO58 is the SPISIMOA.
GPIO_setMasterCore(58, GPIO_CORE_CPU2);
GPIO_setPinConfig(GPIO_58_SPISIMOA);
GPIO_setDirectionMode(58, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(58, GPIO_PIN_TYPE_STD);
// GPIO59 is the SPISOMIA.
GPIO_setMasterCore(59, GPIO_CORE_CPU2);
GPIO_setPinConfig(GPIO_59_SPISOMIA);
GPIO_setDirectionMode(59, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(59, GPIO_PIN_TYPE_STD);
// GPIO60 is the SPICLKA.
GPIO_setMasterCore(60, GPIO_CORE_CPU2);
GPIO_setPinConfig(GPIO_60_SPICLKA);
GPIO_setDirectionMode(60, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(60, GPIO_PIN_TYPE_STD);
// GPIO61 is the SPISTEA.
GPIO_setMasterCore(61, GPIO_CORE_CPU2);
GPIO_setDirectionMode(61, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(61, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(61, GPIO_QUAL_SYNC);
Interrupt_initModule();
Interrupt_initVectorTable();
//
// grant memory access to cpu2
//
MemCfg_setGSRAMMasterSel(MEMCFG_SECT_GS7 | MEMCFG_SECT_GS8 |
MEMCFG_SECT_GS9 | MEMCFG_SECT_GS10, MEMCFG_GSRAMMASTER_CPU2);
//
// Hand-over the SPI module access to CPU2
//
SysCtl_selectCPUForPeripheral(SYSCTL_CPUSEL6_SPI, 1, SYSCTL_CPUSEL_CPU2);