This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: 初上电时,GPIO30管脚为高电平,持续200ms

Part Number: TMS320F28335

MCU初上电时,GPIO30管脚输出高电平,预期为低电平,想知道原因是什么?问题描述如下:

1)MCU初上电时,GPIO30管脚为高电平,持续200ms,同时测量了MCU的1.8V和3.3VIO供电顺序,如图1。

2)在CCS工程软件中,GPIO30配置为无上拉、输出模式,配置后立即CLEAR了该管脚,GPIO的配置软件紧挨着放在在PLL和外设时钟配置之后。

3)硬件上GPIO30和3.3V、GND之间无上拉或下拉电阻,处于浮空状态。

4)更改硬件,在GPIO30和GND之间加2k下拉电阻,测试波形如图2,可见上电时仍有一个200ms的0.64V的电平台阶,虽然该台阶电平较低,但也说明在这个阶段GPIO30仍有0.3mA的驱动能力。

     图1          图2

x 出现错误。请重试或与管理员联系。