Part Number: TIDA-010210
Other Parts Discussed in Thread: ISO7741
TIDA-010210上高压前检测问题.docxTIDA-010210-GaN电源问题.docxTIDA-010210-GaN使能问题.docx
您好,我的问题见附件,目前已经把TIDA-010210样品做出来了,在上高压之前想要初步验证一下系统软硬件。
问题1:
如果要在系统不上高压的情况下初步验证:使TIDA-010210输出50Hz的交流电压,是否在直流端可以连接一个24V电压作为输入,如果不可以,是否还是需要在直流端连接800V电压作为输入?三相负载端是否可以空载?
问题2:
如果要在系统不上高压的情况下使TIDA-010210输出50Hz的交流电压,软件上需要进行什么调整和修改吗?
问题3:
软件的故障检测内容中,fault_DSATA、fault_DSATB、fault_DSATC、fault_vRef1、fault_vRef2分别代表什么?
问题4:
GaN板需要12V供电,而MB板上并未设计给GaN板供电的12V电源,我的解决办法是将GaN板的12V供电脚引到了和主板供电12V共用,经验证GaN工作正常,故障诊断脚输出高电平,请问这样是否可行。
问题5: