This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、XDS110硬件连接:如下图中的两个端口都需要连接
AUX.FUNCYTONS 端口内包含对外供电的信号: TGTSUPPLYOUT 和 GND
DEBUG 端口内包含JTAG相关信号:例如2pin模式下需要连接 1 TMS、 5 VTREF、8 GND、11、TCK
之前以为供电是DEBUG端口的5VTREF和 8GND,就只连接了DEBUG端口,外部供电时烧录程序能正常执行,修改为XDS110供电模式时,烧录一直不成功。
2、软件配置如下
这样配置,就可以使用XDS110对目标板供电(无需外部供电)执行程序烧录了
感谢您对TI产品的关注!
关于你的咨询, 现在XDS110为目标板供电配置成功了吗?
下面的帖子跟您的问题类似你看下。
e2echina.ti.com/.../tms320f280049c-xds110
另外,这是XDS110的用户手册,你可以看看connector的端口配置图。
www.ti.com/.../sprui94.pdf
已经成功了,上面https://e2echina.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/799757/tms320f280049c-xds110帖子也是我发的,之前没有成功就是因为没有接AUX.FUNCYTONS 端口内包含对外供电,以为供电是DEBUG端口的5VTREF和 8GND。