Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
我在sysconfig tool中将RAMLS3配置为共享区域,将RAMLS4配置为CLA程序区域,其余LS区域配置为CPU区域,生成的board.c相关程序如下:
//*****************************************************************************
//
// CLA Configurations
//
//*****************************************************************************
void myCLA0_init(){
//
// Configure all CLA task vectors
// On Type-1 and Type-2 CLAs the MVECT registers accept full 16-bit task addresses as
// opposed to offsets used on older Type-0 CLAs
//
#pragma diag_suppress=770
//
// CLA Task 1
//
CLA_mapTaskVector(myCLA0_BASE, CLA_MVECT_1, (uint16_t)&Cla1Task1);
CLA_setTriggerSource(CLA_TASK_1, CLA_TRIGGER_SOFTWARE);
#pragma diag_warning=770
//
// Enable the IACK instruction to start a task on CLA in software
// for all 8 CLA tasks. Also, globally enable all 8 tasks (or a
// subset of tasks) by writing to their respective bits in the
// MIER register
//
CLA_enableIACK(myCLA0_BASE);
CLA_enableTasks(myCLA0_BASE, CLA_TASKFLAG_1 );
}
void CLA_init()
{
#ifdef _FLASH
#ifndef CMDTOOL // Linker command tool is not used
extern uint32_t Cla1ProgRunStart, Cla1ProgLoadStart, Cla1ProgLoadSize;
extern uint32_t Cla1ConstRunStart, Cla1ConstLoadStart, Cla1ConstLoadSize;
//
// Copy the program and constants from FLASH to RAM before configuring
// the CLA
//
memcpy((uint32_t *)&Cla1ProgRunStart, (uint32_t *)&Cla1ProgLoadStart,
(uint32_t)&Cla1ProgLoadSize);
memcpy((uint32_t *)&Cla1ConstRunStart, (uint32_t *)&Cla1ConstLoadStart,
(uint32_t)&Cla1ConstLoadSize );
#endif //CMDTOOL
#endif //_FLASH
myCLA0_init();
}
//*****************************************************************************
//
// MEMCFG Configurations
//
//*****************************************************************************
void MEMCFG_init(){
//
// Initialize RAMs
//
MemCfg_initSections(MEMCFG_SECT_MSGCPUTOCLA1);
MemCfg_initSections(MEMCFG_SECT_MSGCLA1TOCPU);
while(!MemCfg_getInitStatus(MEMCFG_SECT_MSGCPUTOCLA1));
while(!MemCfg_getInitStatus(MEMCFG_SECT_MSGCLA1TOCPU));
//
// Configure LSRAMs
//
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS0, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS1, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS2, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS3, MEMCFG_LSRAMCONTROLLER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS3, MEMCFG_CLA_MEM_DATA);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS4, MEMCFG_LSRAMCONTROLLER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS4, MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS5, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS6, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS7, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
//
// Configure GSRAMs
//
//
// Configure Access Protection for RAMs
//
MemCfg_setProtection(MEMCFG_SECT_LS0, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_LS1, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_LS2, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_LS3, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_LS4, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_LS5, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_LS6, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_LS7, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE);
MemCfg_setProtection(MEMCFG_SECT_GS0, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE | MEMCFG_PROT_ALLOWDMAWRITE);
MemCfg_setProtection(MEMCFG_SECT_GS1, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE | MEMCFG_PROT_ALLOWDMAWRITE);
MemCfg_setProtection(MEMCFG_SECT_GS2, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE | MEMCFG_PROT_ALLOWDMAWRITE);
MemCfg_setProtection(MEMCFG_SECT_GS3, MEMCFG_PROT_ALLOWCPUFETCH | MEMCFG_PROT_ALLOWCPUWRITE | MEMCFG_PROT_ALLOWDMAWRITE);
//
// Lock/Commit Registers
//
//
// Enable Access Violation Interrupt
//
//
// Correctable error Interrupt
//
MemCfg_setCorrErrorThreshold(0);
MemCfg_disableCorrErrorInterrupt(MEMCFG_CERR_CPUREAD);
}
CMD文件如下:
CLA_SCRATCHPAD_SIZE = 0x100;
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x0000F6, length = 0x00030A
RAMLS02 : origin = 0x008000, length = 0x001800
// RAMLS0 : origin = 0x008000, length = 0x000800
// RAMLS1 : origin = 0x008800, length = 0x000800
// RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
// FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
// FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC123 : origin = 0x081000, length = 0x003000 /* on-chip Flash */
// FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000 /* on-chip Flash */
/* BANK 1 */
FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0 /* on-chip Flash */
// FLASH_BANK1_SEC15_RSVD : origin = 0x09FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x002000
// RAMGS1 : origin = 0x00E000, length = 0x002000
// RAMGS2 : origin = 0x010000, length = 0x002000
DataRam : origin = 0x00E000, length = 0x004000
RAMGS3 : origin = 0x012000, length = 0x001FF8
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
// RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0, ALIGN(4)
.text : >> FLASH_BANK0_SEC4 | FLASH_BANK0_SEC5 | FLASH_BANK0_SEC6 | FLASH_BANK0_SEC7, PAGE = 0, ALIGN(4)
.cinit : > FLASH_BANK0_SEC123, PAGE = 0, ALIGN(4)
.switch : > FLASH_BANK0_SEC123, PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
.paratable : > FLASH_BANK0_SEC15, PAGE = 0
#if defined(__TI_EABI__)
.init_array : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4)
.bss : > RAMLS5, PAGE = 1
.bss:output : > RAMLS02, PAGE = 0
.bss:cio : > RAMLS02, PAGE = 0
.data : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
/* Initalized sections go in Flash */
.const : > FLASH_BANK0_SEC6, PAGE = 0, ALIGN(4)
#else
.pinit : > FLASH_BANK0_SEC123, PAGE = 0, ALIGN(4)
.ebss : >> RAMLS6 | RAMLS7 | RAMGS0, PAGE = 1
.esysmem : > RAMLS5, PAGE = 0
.cio : > RAMLS02, PAGE = 0
.econst : > FLASH_BANK0_SEC6, PAGE = 0, ALIGN(4)
#endif
ramgs0 : > RAMGS0, PAGE = 1
// ramgs1 : > RAMGS1, PAGE = 1
DmaRecvBufFile : > RAMGS3, PAGE = 1
databuf : > DataRam PAGE = 1
/********************CLA************************/
#if defined(__TI_EABI__)
/* CLA specific sections */
Cla1Prog : LOAD = FLASH_BANK0_SEC10,
RUN = RAMLS4,
LOAD_START(Cla1ProgLoadStart),
RUN_START(Cla1ProgRunStart),
LOAD_SIZE(Cla1ProgLoadSize),
PAGE = 0, ALIGN(4)
#else
/* CLA specific sections */
Cla1Prog : LOAD = FLASH_BANK0_SEC10,
RUN = RAMLS4,
LOAD_START(_Cla1ProgLoadStart),
RUN_START(_Cla1ProgRunStart),
LOAD_SIZE(_Cla1ProgLoadSize),
PAGE = 0, ALIGN(4)
#endif
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
/************************************************/
#if defined(__TI_EABI__)
.TI.ramfunc : LOAD = FLASH_BANK0_SEC123,
RUN = RAMLS02,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
GROUP
{
.TI.ramfunc
{ -l F021_API_F28004x_FPU32.lib}
} LOAD = FLASH_BANK0_SEC123,
RUN = RAMLS02,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
/********************CLA************************/
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > RAMLS3, PAGE = 0
.scratchpad : > RAMLS3, PAGE = 0
.bss_cla : > RAMLS3, PAGE = 0
Cla1DataRam : > RAMLS3, PAGE = 0
cla_shared : > RAMLS3, PAGE = 0
CLADataLS1 : > RAMLS3, PAGE = 0
#if defined(__TI_EABI__)
.const_cla : LOAD = FLASH_BANK0_SEC10,
RUN = RAMLS3,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
PAGE = 0, ALIGN(4)
#else
.const_cla : LOAD = FLASH_BANK0_SEC10,
RUN = RAMLS3,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
PAGE = 0, ALIGN(4)
#endif
CLA1mathTables : LOAD = FLASH_BANK0_SEC10,
RUN = RAMLS3,
LOAD_START(_Cla1TablesLoadStart),
LOAD_END(_Cla1TablesLoadEnd),
RUN_START(_Cla1TablesRunStart),
PAGE = 0
/************************************************/
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
在程序中,定义了结构体strVoltPiCtrl,并将其放到了“CLADataLS1”中,同时在100kHz的PWM中断中使用软件触发的形式触发CLAtask1,
CLA_forceTasks(myCLA0_BASE,CLA_TASKFLAG_1);
并试图在PWM中断中对结构体的某些值进行修改,并在CLA中通过这些值进行进一步的计算,并将结果幅值给结构体中的另外一些元素
#pragma DATA_SECTION(strVoltPiCtrl,"CLADataLS1"); PI_CTRL_MODULE strVoltPiCtrl;
结果在进行Debug时,发现结构体strVoltPiCtrl所处的内存区域为Program区域
![]()
导致在Debug模式下,必须先手动connect CLA核,整体程序才能运行,若将程序烧写到Flash,则整体程序将无法运行
经过测试,将100kHz中断中的软件触发CLA屏蔽,或者将PWM中断中屏蔽与该结构体相关的语句,再将程序烧写到FLASH后,则程序又能正常运行,
请问:1.为什么结构体所对应的内存区域为program区域;2.程序为何无法正常运行