This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: DCSM加密后仿真器无法连接

Part Number: TMS320F28P650DK

我通过添加dcsm.cmd和dcsm.asm文件来进行加密,烧录成功后,重新给板子上电,用XDS200仿真器连接,每次连接都是弹出下图的故障,请问有哪些可能或原因,谢谢

     .sect "dcsm_otp_z1_linkpointer"
      .retain
      .long 0x00003FFF
      .long 0x00003FFF
      .long 0x00003FFF
    
     .sect "dcsm_otp_z1_jlm_enable"
      .retain
      .long 0xFFFF0000     ;Z1OTP_JLM_ENABLE
     .sect "dcsm_otp_z1_jtag_pswdh"
      .retain
      .long 0x01234567     ;Z1OTP_JTAGPSWDH0
      .long 0x03678901     ;Z1OTP_JTAGPSWDH1
;;
;;     .sect "dcsm_otp_z1_cmac_key"
;;      .retain
;;      .long 0x00000000     ;Z1OTP_CMACKEY0
;;      .long 0x00000000     ;Z1OTP_CMACKEY1
;;      .long 0x00000000     ;Z1OTP_CMACKEY2
;;      .long 0x00000000     ;Z1OTP_CMACKEY3
;;  
     .sect "dcsm_otp_z1_pswdlock"
      .retain
      .long 0xFB7FFFF0
      
     .sect "dcsm_otp_z1_crclock"
      .retain
      .long 0x7FFFFFFF
   
;;     .sect "dcsm_otp_z1_gpreg"
;;      .retain
;;      .long 0x5AFFFFFF     ;Z1OTP_GPREG1 = Z1_BOOTPIN
;;      .long 0x5AFFFFff     ;Z1OTP_GPREG2
;;      .long 0xFFFFFF00     ;Z1OTP_GPREG3 = Z1OTP_BOOTDEF_LOW
;;      .long 0xFFFFFFFF     ;Z1OTP_GPREG4 = Z1OTP_BOOTDEF_HIGH
     .sect "dcsm_zsel_z1"
      .retain
      .long 0x20FFFFFF     ;Z1OTP_CSMPSWD0 (LSW of 128-bit password)
      .long 0x0123FFFF     ;Z1OTP_CSMPSWD1
      .long 0x0FFFFFFF     ;Z1OTP_CSMPSWD2
      .long 0xFEEEEEEE     ;Z1OTP_CSMPSWD3 (MSW of 128-bit password)
 
      .long 0x55555555     ;Z1OTP_GRABSECT1
      .long 0x55555555     ;Z1OTP_GRABSECT2
      .long 0x55555500     ;Z1OTP_GRABSECT3
      .long 0x00005555     ;Z1OTP_GRABRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved
 
      .long 0xFFFFFFFF     ;Z1OTP_EXEONLYSECT1
      .long 0x0000FFF0     ;Z1OTP_EXEONLYSECT2
      .long 0x000000FF     ;Z1OTP_EXEONLYRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0x60806688     ;Z1OTP_JTAGPSWDL0
      .long 0x0125A2B5     ;Z1OTP_JTAGPSWDL1    


;----------------------------------------------------------------------

; For code security operation,after development has completed, prior to
; production, all other zone select block locations should be programmed
; to 0x0000 for maximum security.        
; If the first zone select block at offset 0x10 is used, the section 
; "dcsm_rsvd_z1" can be used to program these locations to 0x0000.
; This code is commented out for development.

;       .sect "dcsm_rsvd_z1"
;        .loop (1e0h)
;              .int 0x0000
;        .endloop


;----------------------------------------------------------------------
; Zone 2
;----------------------------------------------------------------------
     .sect "dcsm_otp_z2_linkpointer"
      .retain
      .long 0x00003FFF
      .long 0x00003FFF
      .long 0x00003FFF

     .sect "dcsm_rsvd_z2"
      .retain
      .long 0xFFFFFFFF     ;Reserved
     .sect "dcsm_otp_z2_pswdlock"
      .retain
      .long 0x1F7FFFFF
      
     .sect "dcsm_otp_z2_crclock"
      .retain
      .long 0x3FFFFFFF
            
;;     .sect "dcsm_otp_z2_gpreg"
;;      .retain
;;      .long 0x5AFF1820     ;Z2OTP_GPREG1 = Z2_BOOTPIN
;;      .long 0x5AFFFFff     ;Z2OTP_GPREG2
;;      .long 0x00000000     ;Z2OTP_GPREG3 = Z2OTP_BOOTDEF_LOW
;;      .long 0xFFFFFFFF     ;Z2OTP_GPREG4 = Z2OTP_BOOTDEF_HIGH
     .sect "dcsm_rsvd1_z2"
      .retain
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved

     .sect "dcsm_zsel_z2"
      .retain
      .long 0xFFFFFFFF     ;Z2OTP_CSMPSWD0 (LSW of 128-bit password)
      .long 0x1F7FFFFF     ;Z2OTP_CSMPSWD1
      .long 0xFFFFFFFF     ;Z2OTP_CSMPSWD2
      .long 0xFFFFFFFF     ;Z2OTP_CSMPSWD3 (MSW of 128-bit password)
 
      .long 0xAAAAAAAA     ;Z2OTP_GRABSECT1
      .long 0xAAAAAAAA     ;Z2OTP_GRABSECT2
      .long 0xAAAAAA00     ;Z2OTP_GRABSECT3
      .long 0x0000AAAA     ;Z2OTP_GRABRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved
 
      .long 0xFFFFFFFF     ;Z2OTP_EXEONLYSECT1
      .long 0x0000FFF0     ;Z2OTP_EXEONLYSECT2
      .long 0x000000FF     ;Z2OTP_EXEONLYRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved
MEMORY
{
PAGE 0 :  /* Program Memory */

   /* Z1 OTP.  Z1 password locations / Flash and RAM partitioning */
   DCSM_OTP_Z1_LINKPOINTER     : origin = 0x78000, length = 0x00006
   DCSM_OTP_Z1_JLM_ENABLE      : origin = 0x78006, length = 0x00002
   DCSM_OTP_Z1_GPREG           : origin = 0x78008, length = 0x00008
   DCSM_OTP_Z1_PSWDLOCK        : origin = 0x78010, length = 0x00002
   DCSM_OTP_Z1_CRCLOCK         : origin = 0x78012, length = 0x00002
   DCSM_OTP_Z1_JTAG_PSWDH      : origin = 0x78014, length = 0x00004
   DCSM_OTP_Z1_CMAC_KEY        : origin = 0x78018, length = 0x00008

   /* DCSM Z1 Zone Select Contents (!!Movable!!) */
   DCSM_ZSEL_Z1_P0             : origin = 0x78020, length = 0x000020

   /* Z2 OTP.  Z2 password locations / Flash and RAM partitioning */
   DCSM_OTP_Z2_LINKPOINTER     : origin = 0x78200, length = 0x00006
   DCSM_OTP_Z2_RSVD            : origin = 0x78206, length = 0x00002
   DCSM_OTP_Z2_GPREG           : origin = 0x78208, length = 0x00008
   DCSM_OTP_Z2_PSWDLOCK        : origin = 0x78210, length = 0x00002
   DCSM_OTP_Z2_CRCLOCK         : origin = 0x78212, length = 0x00002
   DCSM_OTP_Z2_RSVD1           : origin = 0x78214, length = 0x0000C
   
   /* DCSM Z2 Zone Select Contents (!!Movable!!) */
   DCSM_ZSEL_Z2_P0             : origin = 0x78220, length = 0x000020

}

SECTIONS
{
   dcsm_otp_z1_linkpointer 	: > DCSM_OTP_Z1_LINKPOINTER		PAGE = 0
   dcsm_otp_z1_gpreg        : > DCSM_OTP_Z1_GPREG		    PAGE = 0, type = DSECT
   dcsm_otp_z1_pswdlock		: > DCSM_OTP_Z1_PSWDLOCK		PAGE = 0
   dcsm_otp_z1_crclock		: > DCSM_OTP_Z1_CRCLOCK			PAGE = 0
   dcsm_otp_z1_jlm_enable   : > DCSM_OTP_Z1_JLM_ENABLE,     PAGE = 0
   dcsm_otp_z1_jtag_pswdh   : > DCSM_OTP_Z1_JTAG_PSWDH,     PAGE = 0
   dcsm_otp_z1_cmac_key     : > DCSM_OTP_Z1_CMAC_KEY,       PAGE = 0, type = DSECT
   dcsm_zsel_z1				: > DCSM_ZSEL_Z1_P0				PAGE = 0

   dcsm_otp_z2_linkpointer	: > DCSM_OTP_Z2_LINKPOINTER		PAGE = 0, type = DSECT
   dcsm_otp_z2_gpreg        : > DCSM_OTP_Z2_GPREG		    PAGE = 0, type = DSECT
   dcsm_otp_z2_pswdlock		: > DCSM_OTP_Z2_PSWDLOCK		PAGE = 0, type = DSECT
   dcsm_otp_z2_crclock		: > DCSM_OTP_Z2_CRCLOCK			PAGE = 0, type = DSECT
   dcsm_rsvd_z2             : > DCSM_OTP_Z2_RSVD,           PAGE = 0, type = DSECT
   dcsm_rsvd1_z2            : > DCSM_OTP_Z2_RSVD1,          PAGE = 0, type = DSECT
   dcsm_zsel_z2				: > DCSM_ZSEL_Z2_P0				PAGE = 0, type = DSECT
}